这个是DATASHEET上的原理图,我想问的是P1和P2的数据发送怎么控制?这个芯片只有I2C和HDQ两种通信方式,是通过他们控制的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个是DATASHEET上的原理图,我想问的是P1和P2的数据发送怎么控制?这个芯片只有I2C和HDQ两种通信方式,是通过他们控制的吗?
是的,LED/COMM Configuration Bits [Bits 0, 1, 2 ] 如果为3 = External LEDs with I2C 控制, 如果为4 = External LEDs with HDQ 控制.
Upon detecting A/D value representing 2.5 V on the VEN pin, External LED mode will transmit the RSOC into an
SN74HC164 (for 2~8 LEDs) or two SN74HC164 devices (for 9~16 LEDs) using a bit-banged approach with RC2 (P1)
as Clock and RC0 (P2) as Data.