This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求讨论

Other Parts Discussed in Thread: TPS40305, TPS54320

你好:
关于电源单输入多输出问题。输入12V  5A,输出1.0V 5A  1.8V  3A   2.5V  3A       3.3V 3A   5V 3A     (以上是数字输出),+-10V 1A    +-5V  1A   2.5V  2A  (模拟输出)。

我是这样想的用tps40305可调电源芯片,制作一个输出10v的电压,然后通过稳压芯片78系列调制出要求输出的电压。对于模拟电源输出,输出端加上线性电源芯片。   这样做合理么?求一种芯片,可以同时输出以上电压的芯片。               
                                                                                                                                                                                                                              ---------------张付彬