This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
要有两个误差放大器。buck电路输入15V左右 输出8V左右 电流1.5A。谢谢
亲;为啥要外置MOS?这个电流级别,一体化的IC综合成本是最低的。
亲;需要同步BUCK还是二极管续流的BUCK?分立及一体的产品都有。
我是做实验要学习下外置MOS管的BUCK电路,是那种二极管续流的BUCK,tl494功耗有点大,请推荐一个功能类似tl494,有两路误差比较器的芯片,谢谢
Hi
类似TL494这样通过2个误差放大器控制的脉宽调制控制芯片非常少的。建议您就用TL494.(还有就是TL549,这样的芯片非常少)