This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCP010505BP

Other Parts Discussed in Thread: DCR010505

这是我应用的电源芯片原理图,输出部分我加入了负载电阻,电阻此处我取的是250欧姆,因为依照下面这个图,负载要达到80%才能达到5.0V的输出。所以负载电阻取的时候必需做实验才能得到。

我现在按照我入下图的电路,输出的电压不是很稳定,做了很多线路板,输出电压都不一致,输出电压在5.1V---5.6V之间不等,而且,一旦输出的负载电阻取小了,会造成芯片发热。

我想确认一下的是:1、负载电阻的阻值大小如何确定。2、你们能不能给推荐一个电路,只要满足的要求就行,我的要求就是输入5V,输出也在5V。3、你也可以在我的电路上看有没有什么问题,给出改进的意见。

  • DCP010505BP是1W的隔离无反馈电源芯片,所以您的输出最大电流是1W除以输出电压,DCP010505BP是5V输出,所以最大输出电流是200mA,   电路推荐见datasheet第十一页, layout推荐见datasheet第十五页。

    因为DCP010505是无反馈的隔离设计,所以输出电压会与负载相关,如上述您截取的电压负载图,如果您要输出是5V, 负载取80%,即160mA, 电阻是5V/160mA=31.25欧姆,如果您需要比较精确的输出电压,可以在后端5V输出增加一个LDO, 或者选已经将LDO集成到芯片内部的DCR010505.

  • DCP产品在75%额定负载情况下,输出电压在规格书规定的范围内。

    如果对输出电压精度要求比较高,可以考虑DCR010505