This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问BQ24450使用时发热严重,测试芯片表面温度大概60°,且充电电流过小是什么原因呢?

Other Parts Discussed in Thread: BQ24450

使用BQ24450芯片通过太阳能光伏板给铅酸电池充电,设计输入电压为34V,最大充电电流为7A,使用芯片手册里的参考电路,芯片通过国外供销商采购,应该是正品。但使用过程中,BQ24450发热严重,测试芯片表面温度大概60°,且充电电流最大只能达到1A,随着温度的升高电流会往下将。请问充电电流过小是芯片发热的原因吗?另外芯片为什么发热这么严重,谢谢!

  • 你好,检查一下:

    电池电压多少?是不是处于预充阶段?

    如果电池电压跟输入电压差很大,会导致晶体管Q_EXT发热很大,从而引起芯片发热,晶体管温度是多少?有没有比芯片还高?

    R_ISNS是多少?由它来计算最大充电电流。

  • 你好,非常感谢你的回复!

    1、电池电压处于Vfloat到Vboost之间,应该处于Imax-chg充电阶段。

    2、输入为太阳能光伏板,充电时电压会被电池电压拉低,压差为3V左右。充电时晶体管的温度温度会比芯片的高,估计在70°左右,加了散热片。

    3、R_ISNS的值为0.036欧,计算最大充电电流为6.94A。

    当断开电池时,芯片也会发热,温度在50°左右,此时三极管没有发热,这种情况是不是不太正常呢,是否是芯片本身的原因呢?

    等待芯片变为常温,接入电池后,刚开始的充电电流大概1A左右,但随着芯片温度升高逐渐下降到0.4A,当用散热片帖着芯片表面时,电流会变大,但最终又会回到0.4A。

    麻烦您再帮忙分析一下,非常感谢。