This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9222使能问题

Other Parts Discussed in Thread: UCD9222, UCD7242

使用Xilinx xc95144xl CPLD对UCD9222的EN1、EN2和RST_N,当CPLD只设置这三个引脚时正常使能。

但是我的板子是有多个电源芯片,我每隔5ms使能一个电源芯片:

1. 使能2.5V

2. 使能UCD9222

3. 使能1.8V

4. 使能1.5V

以上1、3、4使能引脚有高电平,但是就是UCD9222的三个使能引脚是低电平。CPLD是One-Hot状态机程序,1状态延迟5MS才能进入2状态,2状态延迟5ms才能进入3状态。

以上情况是在UCD9222是烧写完程序的情况下测试的。

我还有一个没有烧写UCD9222程序的UCD9222+UCD7242模块,同样的程序可按照我上述状态机的顺序,电源全部使能。

请问TI工程师我的问题出在什么地方了