This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH08T240W发烫严重的问题

Other Parts Discussed in Thread: PTH08T240W

大家好,我正在使用PTH08T240W给我的设备供电,这是我做的电路板:

目前空载的时候,输出是5V,正常,发热量特别严重,我后来怀疑是否我焊接有问题,重新焊了一个电源模块的最小系统,发现仍旧发热严重,

这是我电路板的原理图:

其中R3和R4都没有焊,

这是我重焊的最小系统的原理图:

其中输入为12V,图中的470uF我都用了220uF的钽电容代替,Rset为169欧。

我觉得可能是我某个地方没有注意到,虚心向大家求助,谢谢大家!

  • 我也遇到这样的问题,TI电源发热的问题也很困扰我。

  • 您好,

    1) PIN10 Track, 如果不用的话,应该接到VI.

    2) 在你重焊的最小系统上,应该加颗22uF的陶瓷电容,尽可能贴近模块的输入PIN角。输入电容不推荐使用钽电容。

    3) PIN11 INH/UVLO, R4设置不是很合理,可以浮空,或则按下列数值选取 See datasheet Page 22.

    4)RTT 和输出电容的容量关系很大,如你原理图所示的话,R3最好OPEN.

    5)发热严重,温度究竟有多高,从规格书中可以看出,在输入12V,输出5V时,See page 9 Figure 3,power dissipation 大概有1.6W,对于这个小模块来说,也会有温升。