This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3671: 电压输出异常

Part Number: LM3671


两块DC-DC工作在一块电路板上,发现异常时其测量结果如下
LM3671MF-3.3芯片的输入电压为5V,输出电压只有2.9V;
LM3671LC-1.2芯片的输入电压为LM3671MF-3.3的输出(2.9V),其输出电压为1.78V;
将LM3671LC-1.2拆除后测试LM3671MF-3.3的输出电压仍异常;LM3671LC-1.2接入正常3.3V的输入其输出同样异常。

LM3671MF-3.3工作时的SW引脚输出波形如下,其中上面黄色的波形是正常的LM3671MF-3.3引脚输出,下面绿色的波形是异常的LM3671MF-3.3引脚输出,其中异常LM3671MF-3.3的占空比明显的降低。

LM3671LC-1.2工作时的SW引脚输出波形如下,其中上面黄色的波形是正常的LM3671LC-1.2引脚输出,下面绿色的波形是异常的LM3671LC-1.2引脚输出,其中异常LM3671LC-1.2的占空比升高。

下图为两块异常的DC-DC在一块板子工作时的波形输出与正常的两块DC-DC在一块板子工作时的波形输出对比。同样黄色的时正常DC-DC的输出,绿色为异常DC-DC的输出,第一张图为正常和异常的LM3671MF-3.3的SW引脚输出对比,第二张图为正常和异常的LM3671LC-1.2的SW引脚输出对比

希望能够定位导致两块DC-DC损坏的原因