请问哪个芯片可做升压电路,5V输入12V(1.5A)输出
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主,LM3481, LM3478,LM2587都可以满足你的输入输出需求。LM2587是simple swither系列,外围电路简单,工作频率固定为100kHz,使用LM3481是个控制器,工作频率可以高达1M,外部MOS都可以自己选,这样可以选择的余地更大,看你的需求是怎么样的了。
Hi
将电路图放上来看看,另外看一些是否是过流保护了。注意输入电容要足够,并且要尽量靠近电感输入端,对于升压芯片,输入电压如果因为输入电容不够或者layout不好而被拉低,是很容易早晨过流保护的。
HI
TI的webench仿真是可以用于电路设计,建议你参照这个电路来做,同时注意一下layout.