Other Parts Discussed in Thread: GPCRB
FAE, 你好!
1. 常温0.2C放电RSOC正常到0,放电终止电压设置为3400mV:

2. 在低温环境下,RSOC跳变41到0,请问下,需要怎么修改参数来修正?

附GG file
LOG原始数据
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
FAE, 你好!
1. 常温0.2C放电RSOC正常到0,放电终止电压设置为3400mV:

2. 在低温环境下,RSOC跳变41到0,请问下,需要怎么修改参数来修正?

附GG file
LOG原始数据
您好,请帮忙解释下,需要怎么设置才能解决这个RSOC 41% 到0跳变的问题?
当前的设置如下,需达成目标放电3.4V RSOC到0,电池满充电压是4.480V:
"Gas Gauging","FD","Set Voltage Threshold","3400","mV"
"Gas Gauging","FD","Clear Voltage Threshold","3500","mV"
"Gas Gauging","FD","Set % RSOC Threshold","0","%"
"Gas Gauging","FD","Clear % RSOC Threshold","5","%"
"Gas Gauging","FC","Set Voltage Threshold","4430","mV"
"Gas Gauging","FC","Clear Voltage Threshold","4400","mV"
"Gas Gauging","FC","Set % RSOC Threshold","100","%"
"Gas Gauging","FC","Clear % RSOC Threshold","99","%"
"Gas Gauging","TD","Set Voltage Threshold","3500","mV"
"Gas Gauging","TD","Clear Voltage Threshold","3550","mV"
"Gas Gauging","TD","Set % RSOC Threshold","6","%"
"Gas Gauging","TD","Clear % RSOC Threshold","8","%"
"Gas Gauging","TC","Set Voltage Threshold","4420","mV"
"Gas Gauging","TC","Clear Voltage Threshold","4390","mV"
"Gas Gauging","TC","Set % RSOC Threshold","100","%"
"Gas Gauging","TC","Clear % RSOC Threshold","99","%"