This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助TI啊 用LM3404HV做的LED驱动不好使



输入55V,输出24V 700MA,7个3WLED串联,为什么我的电压加到20V时,输出电流0.20A,但是继续加电压,灯的亮度就变了,输出电流减小了,输入电流减小到0.03A了,输出电压变化到18.6V左右,求解释啊!

  • 亲;CS需要用低常数的RC滤波。否则会被干扰而输出异常。

  • 我现在加了一个1K的电阻和471K的电容,电流能加到600MA,在输入电压26.7V的情况下,但是电压继续加大,电流还是减小了很多,在电压加到27V时,板子还有声音了。我设置的频率是500K,之后我把容值换成101,但是电流就只能加到200MA,在输出26.7V的情况下,还是加不到55v,求解释啊

  • 我现在加了一个1K的电阻和471K的电容,电流能加到600MA,在输入电压26.7V的情况下,但是电压继续加大,电流还是减小了很多,在电压加到27V时,板子还有声音了。我设置的频率是500K,之后我把容值换成101,但是电流就只能加到200MA,在输出26.7V的情况下,还是加不到55v,求解释啊