This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: PF status 已编程到 OTP 中是否可以解除

Part Number: BQ76952


您好,

請問BQ76952 如 PF status 已编程到 OTP 中,是否可以解除繼續正常使用FET?

  • 您好,可以解除PF并且正常使用

    • Enter CONFIG_UPDATE_MODE
    • Write all of their settings
    • Read OTP_WR_CHECK to check if OTP programming is okay
    • Send the OTP_WRITE() command 
    • wait 100ms for OTP to program
    • Set PF_EN = 0 in RAM
    • Exit CONFIG_UPDATE_MODE