现在需要使用bq24073给系统锂电池充电,但是当连接电源适配器时bq24073 固定输出4.4V(范围4.3-4.5V)超出系统供电范围(3.4-4.4V, 2A),请问有没有什么器件或电路使电压降低0.15V左右,最好是当连接电源适配器时有压降,没有电源适配器时没压降,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在需要使用bq24073给系统锂电池充电,但是当连接电源适配器时bq24073 固定输出4.4V(范围4.3-4.5V)超出系统供电范围(3.4-4.4V, 2A),请问有没有什么器件或电路使电压降低0.15V左右,最好是当连接电源适配器时有压降,没有电源适配器时没压降,谢谢。
连接适配器时有压降,不连接没有压降什么意思呢?0.15V,貌似肖特基二极管差不多有这个压降。
楼主的意思怎么有点模糊呢,固定输出不是4.4V么?系统供电范围不是3.4~4.4V么?哪儿超出范围了呢?难道有裕量?再说电压降低0.15V,直接加个什么电阻啊
你好,bq24073输出范围是4.3-4.5V,所以有可能超出系统最大工作电压4.4V。
连接电源适配器时bq24073输出4.4V,不连接时输出的是锂电池电压,所以希望在连接适配器时有压降,不连接时没有压降,充分利用电池电量。