TI专家好,
请问TI有没有与附件ADP5062功能相似的芯片,请帮忙推荐一款;
1.带有路径管理功能;
2.可以设置电池电压到一定门限值时,禁止系统电压输出;
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问你的芯片用在什么样的产品上?
我们这边有很多重放电管理芯片,目前用得比较火的有bq24296,BQ24196等,不知道能不能满足你的需求
Jason,
您好!要求支持适配器充电,类似于ADP5062,通过I2C总线设置弱电池电压阈值,使用SYS_EN引脚来关闭系统,不让电池再放电;
现在就是想找这样一款IC,可以进行设置,当电池电压低于一定值时,关闭电池放电回路,电池不再放电;
谢谢!
请TI的工作人员给我推荐一个电池的充放电芯片,放电可以达到5V输出。
===========================================================================================================
我的应用场景是:
我的电池是1节锂电池,2000mA左右。
我的模块电源是5V输出,最大输出700mA电流。
1、当模块电源有电的时候,给电池充电。这个时候模块电源是5V,最大700mA,给电池充电需要降压吗?电池一般是3.7V到4.2V
2、当模块模块电源没有电的时候,电池给模块供电,模块工作最大工作电流500mA。这个时候电池给模块供电需要升压吗,因为模块需要5V电压。
您好,请问你需要这个功能是用来保护电池么? 一般锂电池包内部有自己的保护IC,可以对过放电进行保护,如果电池包内部没有,也是需要一颗IC来完成完整的过冲过放保护,短路保护等功能,BQ29700.
如果是监控系统电压来使能处理器或者MCU一类的电路的话,可以使用专门的supervisor芯片,比如TPS3897
charger的话我们的BQ24296 内部集成了BATFET,与ADP5062类似,是隔离电池和系统的一个JFET,当电池电压较低,2,5V时,自动关断系统电压。这个管子的通断还可以通过I2C来设置。
BQ24296是开关型的,效率更高,这样热的问题容易解决一些。
ning
您好,可以使用BQ24157来实现你的功能,如果你的系统输入5V和输出5V不需要同时存在的话。
BQ24157是一颗需要MCU来控制的IC,如果不想使用MCU的话,可以使用BQ24045来充电,然后使用一颗boost IC tps61028来将电池电压升高到5V
谢谢