BQ32000做出样机发现RTC时钟不稳定,部分机器不能起振。在晶体选型的时候未考虑ESR,采用匹配电容为12.5pf的贴片晶体,ESR值为最大55KOHm。开始怀疑是负载电容焊错,结果发现去掉负载电容后晶体可以起振了,重新焊上22pf电容还是不能起振。
问题:在BQ32000数据手册中有个参数RS :Crystal series resistance 最大值为 40 kΩ,这个参数是否与我们通常理解的ESR一致?如果不一致那么BQ32000能够驱动的最大ESR是多少,如果这就是对晶体ESR的限制,那么是否有较为简便的方法匹配晶体的ESR使得电路稳定。
还请给予解答,谢谢