您好!我正在使用LM5035,有个问题想请问下:LM5035是否可以用于输入电压为120V的情况?看他的数据手册有提供输入电压大于100V时的供电连接方式,但是我在使用中当输入电压大于等于120V时会发生芯片损坏,电路故障的情况,自己认为是电压高于了HB的最大电压118V。所以有这样的疑问:LM5035是否可以用于输入电压高于120V的情况?求各位帮忙啦!!!万分感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主,芯片HS最大的耐压值是105V,而HB引脚最大电压可以承受到118V,都不能达到120V,所以芯片坏是正常的。HB引脚的耐压值高一些,是因为为了驱动上管,需要在HB引脚和HS引脚之间外接一个BOOT电容,通过给BOOT电容充电,来达到给上管提供悬浮驱动的目的,因此HB的电压会比HS电压要高一些,而能够承受的最大电压值也是HB更高一些。至于你提到的那个电路,在VIN>100V的应用,更多的是从芯片的效率和发热的角度来考虑。因为芯片内部的基准电压,VREG电压(5V)是通过内部的线性调压器来实现的,当输入电压太高时,这个线性稳压结构的损耗会比较大,芯片发热比较严重,因此我们会使用手册中提到的电路,把VIN的电压降下来,或者使用辅助绕组来给VIN和VCC供电。所以LM5035不能用在这里。
谢谢了,因为看到专门给有个大于100V输入的Vin接法,所以想多了O(∩_∩)O~
您好,我想请问下,我准备这么做:LM5035的Vin采取推荐的那种大于100V的接法,接为适用于推挽拓扑的驱动方式(即不将HO自举上去),输出的HO和LO再通过IR2110实现悬浮驱动或者变压器自驱,实现半桥DC/DC变换器。具体有几点疑问:
这种情况下HS和HB脚都不会承受超过其最大值的电压,导致LM5035烧毁,但当输入电压达到120V时,采用大于100V的Vin接法,是否会引起芯片其他地方损坏,比如Ramp脚,这个一般是直接与实际Vin通过一个电阻相连的。
此外想请问TI有没有适用于100V输入以上的控制芯片推荐?谢谢了!