This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B4250-Q1應用請教

Other Parts Discussed in Thread: TPS7B4250-Q1

各位好,

小弟有關於TPS7B4250-Q1應用的問題想要請教大家,

現在在設計一個電路輸入12V需要輸出電壓+5V的Accuracy (%)越小越好,

所以選用了TPS7B4250-Q1,但是此IC還需要提供一個ADJ/EN電源,

想要請問一下各位,如果我只是要轉出+5V,應該如何設計相關電路?麻煩大家了,謝謝!!!

  • 亲;只是需要固定5V;选这个IC太麻烦了。推荐TPS7B6750B-Q1,这两个IC的标准等级是一样的。

  • Hardy,

    其实TPS7B4250-Q1就是针对

    需要很高精度的参考电压,但是此时,由于参考电压芯片的带负载能力通常非常的小,所以需要TPS7B4250-Q1提供相对较高的电流。TPS7B4250-Q1理论上支持最高50mA,取决于环境温度。

    通常需要在ADJ提供一个精度很高的参考供电。TPS7B4250-Q1的输出精度也取决于这个参考供电芯片的精度。

    应用框图如下:

    谢谢。