This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3405A输出问题

Other Parts Discussed in Thread: LM3405A, LM3405

想请问一下:: LM3405A额定输出电流1A是否能长时间维持1A不变吗???

  • 顶一下,盼高手回复

  • 您好,光就芯片本身的耐流能力而言是可以的。

    但这里有另外一个问题是芯片的散热及温升,因LM3405的热阻为118C/W,要看下您输入电压/输出电压,所设定频率等来计算下芯片的损耗(详见规格书第16页,一般而言,输入电压和频率越高,输出电流越大会导致越大的损耗),然后就该损耗再看下典型LAYOUT下的温升,最后要热学设计上看看是否需要用其他方法来降低温升(一般建议您芯片温升不超过50C)

    如满足上述温升条件的话应用是可以的,但一般高压/高频应用时1A输出,仅用PCB散热的话(铝基板除外)估计温升会有问题。

     

  • 亲;不知道亲是问这IC是否能长时间输出1A还是无论负载,保持1A输出?

    如前面所诉,是否能长期1A工作;由散热条件决定。至于后半个问题,这是稳压IC;不稳流。

  • 输入电压是10~18VAC,输出电压为10V/1A,,负载9个1WLED,整灯外铝壳温度是65度左右,,,谢谢,,帮忙看看能否维持1A电流不变!

  • 输入电压是10~18VAC,输出电压为10V/1A,,负载9个1WLED,整灯外铝壳温度是65度左右,,,谢谢,,帮忙看看能否维持1A电流不变!另输入交流或直流,哪种会更好!