用LM3405A做LED驱动,,输入电压是10~18VAC,输出电压为10V/1A,,负载9个1WLED,整灯外铝壳温度是65度左右,,,帮忙看看输出能否维持1A电流不变!另输入为交流或直流,哪种会更好!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输入12~18VAC或DC30V,输出10V/1A额定负载 ,,同类型的有没其他型号推荐,,低成本线路简单点的!感谢
有DC30V输入的话,可以看一下LM3404,输入电压最高42V,额定电流也是1A,线路非常简单,外围器件也没几个。
网上的价格只是一个参考,而且LM3405A无法满足你的设计要求,在你的case里这两个IC没有可比性啊。