This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI专家好,
现在用LM27313来做一款LCD升压背光电路,要求输出19.2V/20mA,想用PWM调光方式,帮忙看看是否可以?
谢谢!
你太有才了,不仅仅是做的电路
亲;使用FB脚就可以低频PWM调光。
Hi
不建议你用这一款芯片LM27313, 而建议你直接采用TI的背光LED方案,例如TPS61160A:
这个方案电路简单,控制容易,输入电压并不仅仅受限3~5V,它的最高输入电压范围是18V.
按照你TPS27313的电路,实际上已经是可以PWM调光的,它是通过将PWM信号滤波成直流影响FB反馈进而达到控制亮度的。