This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2057芯片使用中发热严重



设计的恒流充电电流为2A。MOS管参数感觉没什么问题,充电器采用的是5V,2A的手机充电器。然后电池是两节并联的三洋18650锂离子电池。

充电时参数:充电器电压4.7V,经二极管后大约4.5V。充电终止电压是4.2V。恒流充电期间,电池的电压从3.7V起,慢慢升高。

现发现恒流充电时,不仅MOS管发热,BQ2057芯片也同样发热,手指无法持续放在上面,温度可能达到了器件的极限工作温度70度以上。

请问是否正常现象?可能的原因是什么?是否该芯片不支持如此大电流的充电?

  • 亲;如果手指长时间放在70C上;可以烫出水泡了^-^。IC和MOSFET在一起;因介质导热而感到烫手是正常现象。建议扩大覆铜面积以利散热。

  • 电路图没有问题,对于改善散热 ,有以下建议供你参考:

    1,确定芯片底部有良好接散热铜箔,对于有设计thermal pad的器件,底部请保持与接地的铜箔焊接良好,有需要时可以在底部打一系列散热孔。

    2,检测所选用的mosfet的散热能力,选择散热性能更好的mosfet(参考其热阻数据)

    3,如果充电时产生的温度还是不能接受,可以考虑在芯片顶端加小型的散热片。

    以上谢谢!