UCC28610芯片手册SLUS888F(2012)第19页,第一段第5-6行:The corner frequency of the filter in Figure 24 should be at least a decade above the
maximum switching frequency of the converter, as given in Equation 11.
中文意思应该是:图24中的滤波器转折频率必须在转换器最大开关频率的10倍以上,该滤波器转折频率由等式11给出。
该芯片最大开关频率133KHz,那么滤波器转折频率应该是其10倍以上,即大于1330KHz。
但是在官方推荐的电路中Rfb = 20.5K ,Cfb = 100 pF,按11式计算Ffb = 77.67KHz,这远远小于1330KHz,
到底是官方这个算法有问题,还是本人的理解出错,求解!!!
附官方推荐电路和芯片手册如下