1. 用TPS7A4700/4701搭建电源模块时是否需要加防止倒流的保护二极管,就是从输入反接到输出,从输出反接到地的两个?
2. TPS7A4700/4701的区别是否就是4701具备用电阻网络的比值来控制输出电压值的功能,而4700只能通过0P1V等可编程引脚控制?那怎么确定4701的控制方式到底是哪一种呢?
谢谢各位大虾!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢哦!
第一个问题,确实没有感性负载,但是不仅仅感性负载时会出现输出端高于输入端需要保护,当电路有很多电容时,断电以后输入端电压消失,输出端电压慢慢才会降下来,这样的话输出端超过输入端,容易损坏内部元件啊,像LM317,LM78XX等一般都要加个二极管的。就是不清楚有没有内部的保护机制,其他保护机制倒是很多,像热关断、限流等等。
第二个问题,4700好像是不能用电阻网络的;4701可以用外置电阻网络,也可以用编程电阻,但要是两个同时用来会怎么样:比如我编程网络配置成15V的,外置电阻网络配置成20V的,输出是多少?