各位TI工程师们,你们好
我公司最近用UCC288061方案做了一个150W的恒压电源,总体上效果还是很不错的 但遇到到了几个问题
1.低压效率低只有80% 220V输入是有89%
2.100V输入是启动较慢,要10秒才能开启
3.空载电压不稳定
请各位工程师帮忙解决 联系电话 13532107394
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.参考EVM板的测试数据,你的效率确实低了点。300W EVM板半载的数据是 92.5%@85Vinrms,96.8%@230Vinrms.PFC的功耗主要在整流桥、MOS、二极管、电感、电解电容上,请考虑你器件是否设计合理。建议把THD和PF指标做好之后再考虑效率,直观地看,电流波形漂亮的话效率也相对优。
2.根据datasheet 21页和你的原理图检查一下软启动的过程,典型的起机波形在EVM文档的第9页。
3.boost电路会有一个与输入电压、负载、电感有关的右半平面零点,补偿器设计的时候注意使穿越频率避开此零点,建议检查环路。
FYI: Datasheet- www.ti.com/.../slus837a.pdf