This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教电源输出信号在打印机开动时出现陷波的问题

Other Parts Discussed in Thread: TPS5450

如题,电源模块是TPS5450组成的19V转8VDC-DC电路,输出电压8V,输出最大电流2A,设计的电路输出电感为47uH,输出电容100uF。

在开启热敏打印机的时候,DC-DC电路输出的8V就会出现明显的陷波,陷波最大能达到2V,陷波周期比较小,大概为1Hz。关闭打印机,陷波就消失。

求教为什么会出现这种情况呢?如何解决这个问题?