bq27510可以监测3节2032纽扣电池吗?本人系统有重量要求,因此采用3个纽扣电池串联供电(10V),现在,想监测电池的电量,用bq27510可以吗??或bq27510的测温接口如果不用是否可以直接悬空?或者有没有其它的更好的3个纽扣电池串联的电量监测方案??yanchenglinglf@163.com
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
bq27510可以监测3节2032纽扣电池吗?本人系统有重量要求,因此采用3个纽扣电池串联供电(10V),现在,想监测电池的电量,用bq27510可以吗??或bq27510的测温接口如果不用是否可以直接悬空?或者有没有其它的更好的3个纽扣电池串联的电量监测方案??yanchenglinglf@163.com
嗯,能不能推荐一个TI的解决方案,关于监测三个CR2032纽扣电池串联电量的方案呢?!
你好,针对纽扣电池目前是没有专业的电量检测方案的,如果是需要一个低电压报警的功能,可以用简单的电压比较器,或者放在负载端的电压检测器来实现简单的更换电池报警功能,详见TI的电源产品列表。谢谢!
3节小容量锂聚合物电池串联的电量管理场合建议您考虑BQ40Z50,以上谢谢!
用3个210mah3.7V聚合物锂电池进行串联,,串联后的电压是11V,,可以用bq40z50可以?
可以的,BQ40Z50 可以支持1到4节电池,请参考其产品主页规格说明以及相关的应用手册了解详细的信息,谢谢。