This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于电量计BQ34Z100的几点疑问,求解答

Other Parts Discussed in Thread: BQ34Z100, BQ27742-G1

目前正在摸索用单片机I2C接口与电量计进行参数设置,有以下疑问:

疑问一:模式转换

seal-unseal,unseal-full模式之间的转换,是向寄存器0x00依次写入4个数据(0xffffffff),还是先向0x00,0x01分别写入0xff后,再次向0x00,0x01分别写入0xff?

为什么我读0x00寄存器的状态一直是0x0004

疑问二:data flash写入

能够读相应位置的data flash数据,也能够通过BLOCKDATA()向32位块FLASH空间写数据,但是不能改变相应位置的data flash数据的值,请问checksum怎么生成?

  • 1.http://www.deyisupport.com/question_answer/analog/battery_management/f/35/t/46539.aspx  这个问题在链接的帖子有描述还有波形参考,向0x00写入0xff,0xff再向0x01写入0xff,0xff

    2.建议采用上位机EVSW配合EV2300/2400进行参数设置,上位机会自动计算checksum数值。单片机checksum可以参考下面的描述

    This byte contains the checksum on the 32 bytes of block data read or written to data flash.
    The least-significant byte of the sum of the data bytes written must be complemented ( [255 – x] , for x the 8-bit
    summation of the BlockData() (0x40 to 0x5F) on a byte-by-byte basis.) before being written to 0x60.

     

  • 我也遇到这个问题了:

    This byte contains the checksum on the 32 bytes of block data read or written to data flash.
    The least-significant byte of the sum of the data bytes written must be complemented ( [255 – x] , for x the 8-bit
    summation of the BlockData() (0x40 to 0x5F) on a byte-by-byte basis.) before being written to 0x60.

    这是手册上的一段话,我按照这个做了,但是值并没有改变啊。

  • 关于dataflash 内容的修改,可以参照http://www.ti.com/lit/ug/sluuac9/sluuac9.pdf 的page11。

    里面可以参照计算方法,和过程,对应的寄存器的值需要和bq34z100对照。

  • 您好,按照你说的方法,成功把DesignedCapacity这个值改变了,谢谢你。

    我用的是BQ27742-G1,又遇到了一个问题:

     FETTest( ): 0x74 and 0x75这个命令,我想把CHG和DSG对应的FET 都打开,

    就给0x74赋0x00

             0x75赋0x83,

    执行START_FET_TEST后,

    0x74状态位仍然是0x00,0x75变成0x01,但是用电表测量后发现两个FET都没有电压。请问这是什么原因?