Hi,all:
使用fusion digital power designer调试UCD9222,直接导入了6678EVM自带的配置好XML工程。
在online模式,已经可以正确输出电压。准备download fireware时,导出.x0文件,却提示需要enable GUI advanced features。而使能这个功能却是需要输入密码。
请问下TI的工程师s,可否给我提供下这个密码,谢谢啦~~
我的EMAIL:bootloading@163.com
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
UCD9xxxx devices come from the factory with the PFlash already installed, you only require the DFlash to be downloaded to the device.
If you are attempting to Export both the Program and Data Flash then have the customer Export just the Data Flash, this does not require the password.
您好:
我在TI官网买的usb interface adapter ,电脑软件安装的是TI-Fusion-Digital-Power-Designer-2.0.166,但是一直连不上我的电路板上的ucd9222,接口定义检查无误,我的ucd9222+ucd7242是按开发板设计,将usb interface adapter断开电路板,测量不到标准的时钟数据信号,请问是不是 usb interface adapter出现问题了呢?谢谢! 附件是具体信息!