具体的应用是USB口要做数据通讯,但是同时希望能对接在上面的手持设备正常智能充电,想法是将TPS2511的DP,DM接到USB host的D+,D-端口,我听说如果这种接法,用TPS2511做USB口充电时,相应的USB口无法和设备通讯,所以只能做USB智能充电,是否对?
如果既要有智能充电,又要使USB口能同时传送数据,是否只能选择TPS2546?--谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,TPS2511是charge only 芯片,如果需要charge & data 可以考虑TPS2546,谢谢。
Frank,多谢
但是我看TPS2511和TPS2546内部结构很类似,只是TPS2546可以通过外部设置充电方式,以及有一对开关来控制D+/D-,其内部的自动检测也是挂到D+/D-数据线上。
那如果我将TPS2511DM/DP通过外部走线并联到D+/D-上,不就和TPS2546内部接线一样了吗?这样的话TPS2511只是检测设备然后选择合适的充电电流。通讯还是通过USB host直接和USB client通讯。是否可行?
因为如果用这种方式,可以根据项目的需求,决定是否提供快速充电还是用普通充电,并且阻抗匹配比较容易,如果用TPS2546,则在USB输入输出端都要做阻抗匹配。
Zhimin,
你提到的一对开关,正是TPS2511不能同时用于充电和数据传输的关键,没有这个开关,不同时段的DM,DP就会发生冲突。所以如果想用2511来实现,可以外加这个开关。TI的BQ24392可以帮你实现。