This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI 有没有低成本和极低功耗的LDO ,要求输出固定3.6V?



你好!想选一款极低功耗,固定输出3.6V,电流100mA左右的LDO,能否推荐一个型号。谢谢!

还有:TI 在没有一款低压降(VF小于0.4V)的小功耗(1A左右)肖特基整流桥?低压差(VF小于0.2V)肖特基二极管?谢谢!

  • 3.6V的LDO可以选TLV70036和TLV70236,  TPS78236, 功耗主要取决与输入电压与输出电压的压差和负载电流的乘积,所以主要在与您选择的输入源。

    TI主要是做芯片的,所以肖特基二极管没有可以推荐的。