This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

POE/ TPS23750pwp

Other Parts Discussed in Thread: TPS23750

 左图为我参考TPS23750的降压电路修改而来,PSE为华为的POE交换机,空载情况下有14.1V输出,但加上负载之后输出电压降为3.8V,用万用表测量IRF510的Vgs为0V,Vfb为0.8V(都不正常),我请问以下几个问题:

1、TPS23750是否与PSE设备有一定的兼容性问题?

2、TPS23750外围元器件是否有严格的参数限制?(图中的MBR1100我用SR1100代替啦)

3、像这种情况,是GATE无法驱动IRF510造成的嘛?(原电路图中为SI2328DS)

      谢谢!

 

Protel Schematic.rar
  • 1.如果标准一致的话,应该是兼容的。芯片采用的是 802.3af,如果PSE也采用该标准,应该是兼容的。

    2.你的图实在看不清,建议发个PDF的附件大家看起来方便一点。器件的参数根据你的规格而定。

    3.你带多大的负载。Vgs为零不是无法驱动mos的问题,是不是触发了保护或者带载情况下检测PD被干扰?

  • 我已上传了一份PDF原理图,你看下,输出电容没有加上去;

    刚才用示波器跟踪MOS管的栅极,有个30MS、15V的电压,之后就什么都没有啦!Vcomp=1.40V,Vfb=1.5V,Vtmr=3.48V(都是空载情况下测的)。