Other Parts Discussed in Thread: GPCRB
What factors will trigger a reset,And What are the effects of resett?
The log shows the BUG described. When it is below 15 degrees Celsius, discharge at a current of around 1A, unlock the electricity meter, click the RESET command, and the SOC will report 100%. After shutting down the machine during the -20 degree test, there was also a 100% battery alarm issue when restarting. Please help confirm the logic triggered by the RESET command.Host check did not actively send reset command
Thu May 04 18:15:11 CST 2023 Device Version Info = 1561_1_03 BQZ Device Name = bq27z561R1 BQZ Firmware Version = 1_03 Sample,DateTime,ElapsedTime,ManufAccess,@Rate(@),@TimeEmpty,Temperature,Voltage,Current,AvgCurr,AvgPow,RSOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeFull,MaxLoadCurrent,MaxLoadTimeEmty,VoltHiSet,VoltHiClear,VoltLoSet,VoltLoClear,TempHiSet,TempHiClear,TempLoSet,TempLoClear,SOCDeltaSet,BTPDsgSet,BTPChgSet,IntStatus,ChgCurr,ChgVolt,MaxCurr,BattStat,CycleCnt,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,CellVolt1,CellCurr1,CellPower1,Power,IntTemp,TS1Temp,CellTemp,Cell1RawV,WkCompI,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,CompRes1,PackGrid,LStatus,CellGrid1,StateTime,DOD0_1,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,QMax1,QMaxDOD0_1,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus 1,2023-05-04 18:15:21,10.014,0x0077,0,65535,-20.8,4261,-74,-77,-33,92,4167,4577,3247,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1233,0x00C0,10,97,0x0380,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4261,-78,-33,-32,-21.4,-20.8,-20.8,4261,-82,4167,1538,4577,1717,3968,1538,343,149,4381,1717,-19.7,-20.8,1000,55,2,14,2,1244,1884,70,30,10,736,4889,672,421,351,10.0,417,1904,4538,1777,957,SUCCESS 2,2023-05-04 18:15:31,20.017,0x0054,0,65535,-20.9,4260,-78,-78,-33,92,4167,4577,3205,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1224,0x00C0,10,97,0x0380,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4260,-78,-33,-33,-21.4,-20.9,-20.9,4260,-78,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-20.9,1000,55,2,14,2,1254,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,909,SUCCESS 3,2023-05-04 18:15:41,30.018,0x0054,0,65535,-20.9,4259,-74,-77,-33,92,4167,4577,3247,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1224,0x00C0,10,97,0x0380,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4259,-78,-33,-32,-21.5,-20.9,-20.9,4259,-78,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-20.9,1000,55,2,14,2,1263,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,909,SUCCESS 4,2023-05-04 18:15:51,40.034,0x0054,0,65535,-21.0,4338,0,-43,-18,92,4167,4577,5814,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1217,0x00C0,10,97,0x0380,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4338,0,0,0,-21.5,-21.0,-21.0,4339,0,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-21.0,1000,55,2,14,2,1273,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,908,SUCCESS 5,2023-05-04 18:16:01,50.039,0x0054,0,65535,-21.0,4343,0,-21,-9,92,4167,4577,11906,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1217,0x00C0,10,97,0x0380,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4343,0,0,0,-21.5,-21.0,-21.0,4344,-4,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-21.1,1000,55,2,14,2,1283,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,953,SUCCESS 6,2023-05-04 18:16:11,60.055,0x0054,0,65535,-21.1,4345,0,-11,-5,92,4167,4577,22729,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1209,0x00C0,10,97,0x0380,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4345,0,0,0,-21.5,-21.1,-21.1,4345,0,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-21.1,1000,55,2,14,2,1293,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,884,SUCCESS 7,2023-05-04 18:16:21,70.068,0x0054,0,65535,-21.1,4345,0,-5,-2,92,4167,4577,50004,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1209,0x00C0,10,97,0x0380,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4345,0,0,0,-21.6,-21.1,-21.1,4345,0,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-21.2,1000,55,2,14,2,1303,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,906,SUCCESS 8,2023-05-04 18:16:31,80.084,0x0054,0,65535,-21.2,4346,0,-3,-1,92,4167,4577,65535,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1202,0x00C0,10,97,0x0380,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4346,0,0,0,-21.6,-21.2,-21.2,4346,-4,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-21.2,1000,55,2,14,2,1313,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,920,SUCCESS 9,2023-05-04 18:16:41,90.088,0x0054,0,65535,-21.2,4346,0,-1,-1,92,4167,4577,65535,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1202,0x00C0,10,97,0x0380,0x0040,0x01,0x0018,0x80,0x4003,0x0008,4346,0,0,0,-21.7,-21.3,-21.2,4346,0,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-21.2,1000,55,2,14,2,1323,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,929,SUCCESS 10,2023-05-04 18:16:51,100.093,0x0054,0,65535,-21.3,4347,0,0,0,92,4167,4577,65535,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1202,0x00C0,10,97,0x8280,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4347,0,0,0,-21.7,-21.3,-21.3,4347,0,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-21.3,1000,55,2,14,2,9,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,955,SUCCESS 11,2023-05-04 18:17:01,110.099,0x0054,0,65535,-21.3,4347,0,0,0,92,4167,4577,65535,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1202,0x00C0,10,97,0x8280,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4347,0,0,0,-21.7,-21.3,-21.3,4347,0,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-21.3,1000,55,2,14,2,19,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,855,SUCCESS 12,2023-05-04 18:17:11,120.113,0x0054,0,65535,-21.4,4347,0,0,0,92,4167,4577,65535,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1202,0x00C0,10,97,0x8280,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4347,0,0,0,-21.7,-21.4,-21.4,4347,0,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-21.4,1000,55,2,14,2,29,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,937,SUCCESS 13,2023-05-04 18:17:21,130.117,0x0054,0,65535,-21.5,4348,0,0,0,92,4167,4577,65535,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1202,0x00C0,10,97,0x8280,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4348,0,0,0,-21.9,-21.5,-21.5,4348,0,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-21.5,1000,55,2,14,2,39,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,857,SUCCESS 14,2023-05-04 18:17:31,140.125,0x0054,0,65535,-21.5,4348,0,0,0,92,4167,4577,65535,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1202,0x00C0,10,97,0x8280,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4348,0,0,0,-21.8,-21.5,-21.5,4348,0,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-21.5,1000,55,2,14,2,49,1884,71,30,10,736,4889,672,422,351,10.0,417,1904,4538,1777,958,SUCCESS 15,2023-05-04 18:17:41,150.135,0x0054,0,65535,-21.6,4348,0,0,0,92,4167,4577,65535,65535,-3872,65,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x10,0,0,1202,0x00C0,10,97,0x8180,0x0040,0x01,0x0018,0x40,0x0718,0x0008,4348,0,0,0,-21.9,-21.6,-21.6,4348,0,4167,1538,4577,1717,3967,1538,343,149,4381,1717,-19.7,-21.6,1000,55,2,14,2,59,1884,71,30,11,736,4889,672,422,352,10.0,417,1904,4538,1777,918,SUCCESS 16,2023-05-04 18:17:51,160.147,0x0054,0,0,-21.6,4348,0,0,0,0,0,4670,0,0,-500,0,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,4450,4450,1170,0x00C0,10,97,0x0300,0x0040,0x00,0x0000,0x40,0x0014,0x0008,4348,0,0,0,-21.9,-22.0,-21.6,4349,0,3926,1520,4351,1704,3926,1520,425,184,4351,1704,-21.6,-21.6,1000,0,0,14,0,0,2176,0,0,0,752,4889,0,0,0,10.0,417,2176,4538,1777,891,SUCCESS 17,2023-05-04 18:18:01,170.154,0x0054,0,65535,-21.6,4348,0,0,0,91,3926,4351,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1170,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4348,0,0,0,-22.0,-21.6,-21.6,4348,0,3926,1520,4351,1704,3926,1520,425,184,4351,1704,-21.6,-21.6,1000,0,0,14,0,10,2176,0,0,0,752,4889,0,0,0,10.0,417,2176,4538,1777,854,SUCCESS 18,2023-05-04 18:18:11,180.159,0x0054,0,65535,-21.7,4349,0,0,0,91,3926,4351,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1170,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4349,0,0,0,-22.0,-21.7,-21.7,4349,0,3926,1520,4351,1704,3926,1520,425,184,4351,1704,-21.6,-21.7,1000,0,0,14,0,20,2176,0,0,0,752,4889,0,0,0,10.0,417,2176,4538,1777,865,SUCCESS 19,2023-05-04 18:18:21,190.175,0x0054,0,65535,-21.7,4349,0,0,0,91,3926,4351,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1170,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4349,0,0,0,-22.0,-21.7,-21.7,4349,0,3926,1520,4351,1704,3926,1520,425,184,4351,1704,-21.6,-21.7,1000,0,0,14,0,30,2176,0,0,0,752,4889,0,0,0,10.0,417,2176,4538,1777,865,SUCCESS 20,2023-05-04 18:18:31,200.176,0x0054,0,65535,-21.8,4349,0,0,0,91,3926,4351,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1170,0x00C0,10,97,0x8200,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4349,0,0,0,-22.0,-21.8,-21.8,4349,0,3926,1520,4351,1704,3926,1520,425,184,4351,1704,-21.6,-21.8,1000,0,0,14,0,40,2176,0,0,0,752,4889,0,0,0,10.0,417,2176,4538,1777,926,SUCCESS 21,2023-05-04 18:18:42,210.827,0x0077,0,65535,-21.8,4349,0,0,0,91,3926,4351,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1170,0x00C0,10,97,0x8100,0x0440,0x01,0x0018,0x40,0x0014,0x0008,4349,0,0,0,-22.1,-21.9,-21.9,4349,-4,3926,1520,4351,1704,3926,1520,425,184,4351,1704,-21.6,-21.8,1000,0,0,14,0,51,2176,0,0,0,752,4889,0,0,0,10.0,417,2176,4538,1777,855,SUCCESS 22,2023-05-04 18:18:51,220.185,0x0054,0,65535,-21.8,4349,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,934,4450,1157,0x00C0,10,97,0x8300,0x0040,0x02,0x0004,0x40,0x0014,0x0008,4349,0,0,0,-22.1,-21.8,-21.8,4349,0,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-21.8,1000,0,0,14,0,4,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,888,SUCCESS 23,2023-05-04 18:19:01,230.201,0x0054,0,65535,-21.9,4349,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1157,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4349,0,0,0,-22.1,-21.9,-21.9,4349,0,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-21.9,1000,0,0,14,0,14,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,889,SUCCESS 24,2023-05-04 18:19:11,240.213,0x0054,0,65535,-21.9,4350,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1157,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4350,0,0,0,-22.2,-21.9,-21.9,4350,-7,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-21.9,1000,0,0,14,0,24,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,893,SUCCESS 25,2023-05-04 18:19:21,250.224,0x0077,0,65535,-21.9,4350,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1157,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4350,0,0,0,-22.2,-21.9,-21.9,4350,0,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-21.9,1000,0,0,14,0,34,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,867,SUCCESS 26,2023-05-04 18:19:31,260.237,0x0077,0,65535,-22.0,4349,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1157,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4349,0,0,0,-22.2,-22.0,-22.0,4349,-7,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-22.0,1000,0,0,14,0,44,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,857,SUCCESS 27,2023-05-04 18:19:41,270.250,0x0077,0,65535,-22.0,4350,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1157,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4350,0,0,0,-22.2,-22.0,-22.0,4350,0,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-22.0,1000,0,0,14,0,54,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,905,SUCCESS 28,2023-05-04 18:19:51,280.254,0x0077,0,65535,-22.0,4350,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1157,0x00C0,10,97,0x8300,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4350,0,0,0,-22.3,-22.0,-22.0,4350,0,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-22.0,1000,0,0,14,0,63,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,854,SUCCESS 29,2023-05-04 18:20:01,290.267,0x0077,0,65535,-22.1,4350,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1157,0x00C0,10,97,0x8300,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4350,0,0,0,-22.3,-22.1,-22.1,4350,4,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-22.0,1000,0,0,14,0,73,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,858,SUCCESS 30,2023-05-04 18:20:11,300.280,0x0054,0,65535,-22.1,4350,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1157,0x00C0,10,97,0x8300,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4350,0,0,0,-22.3,-22.1,-22.1,4350,-4,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-22.1,1000,0,0,14,0,83,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,894,SUCCESS 31,2023-05-04 18:20:21,310.288,0x0054,0,65535,-22.1,4349,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1157,0x00C0,10,97,0x8300,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4349,0,0,0,-22.3,-22.1,-22.1,4349,-7,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-22.1,1000,0,0,14,0,93,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,869,SUCCESS 32,2023-05-04 18:20:31,320.293,0x0054,0,65535,-22.1,4350,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1157,0x00C0,10,97,0x8300,0x0440,0x00,0x4083,0x40,0x0034,0x0008,4350,0,0,0,-22.3,-22.1,-22.1,4350,-7,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-22.1,1000,0,0,14,0,103,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,957,SUCCESS 33,2023-05-04 18:20:41,330.304,0x0054,0,65535,-22.1,4350,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1157,0x00C0,10,97,0x8200,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4350,0,0,0,-22.3,-22.0,-22.0,4350,-7,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-22.1,1000,0,0,14,0,113,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,902,SUCCESS 34,2023-05-04 18:20:51,340.313,0x0054,0,65535,-22.1,4350,0,0,0,91,3928,4346,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1157,0x00C0,10,97,0x8100,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4350,0,0,0,-22.3,-22.1,-22.1,4350,0,3928,1521,4346,1702,3928,1521,418,181,4346,1702,-21.8,-22.1,1000,0,0,14,0,123,2160,0,0,0,760,4889,0,0,0,10.0,417,2160,4538,1777,894,SUCCESS 35,2023-05-04 18:21:01,350.316,0x0054,0,65535,-22.1,4350,0,0,0,91,3926,4337,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,934,4450,1137,0x00C0,10,97,0x8300,0x0040,0x02,0x0004,0x40,0x0014,0x0008,4350,0,0,0,-22.3,-22.1,-22.1,4350,-4,3926,1520,4337,1698,3926,1520,411,178,4337,1698,-22.1,-22.1,1000,0,0,14,0,2,2144,0,0,0,768,4889,0,0,0,10.0,417,2144,4538,1777,892,SUCCESS 36,2023-05-04 18:21:11,360.318,0x0054,0,65535,-22.2,4350,0,0,0,91,3926,4337,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1137,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4350,0,0,0,-22.3,-22.2,-22.2,4350,4,3926,1520,4337,1698,3926,1520,411,178,4337,1698,-22.1,-22.2,1000,0,0,14,0,12,2144,0,0,0,768,4889,0,0,0,10.0,417,2144,4538,1777,858,SUCCESS 37,2023-05-04 18:21:21,370.322,0x0054,0,65535,-22.1,4350,0,0,0,91,3926,4337,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1137,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4350,0,0,0,-22.3,-22.1,-22.1,4350,-4,3926,1520,4337,1698,3926,1520,411,178,4337,1698,-22.1,-22.1,1000,0,0,14,0,22,2144,0,0,0,768,4889,0,0,0,10.0,417,2144,4538,1777,870,SUCCESS 38,2023-05-04 18:21:31,380.328,0x0054,0,65535,-22.3,4350,0,0,0,91,3926,4337,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1137,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4350,0,0,0,-22.3,-22.3,-22.3,4350,4,3926,1520,4337,1698,3926,1520,411,178,4337,1698,-22.1,-22.3,1000,0,0,14,0,32,2144,0,0,0,768,4889,0,0,0,10.0,417,2144,4538,1777,895,SUCCESS 39,2023-05-04 18:21:41,390.342,0x0054,0,65535,-22.3,4350,0,0,0,91,3926,4337,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1137,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4350,0,0,0,-22.4,-22.3,-22.3,4350,-4,3926,1520,4337,1698,3926,1520,411,178,4337,1698,-22.1,-22.3,1000,0,0,14,0,42,2144,0,0,0,768,4889,0,0,0,10.0,417,2144,4538,1777,864,SUCCESS 40,2023-05-04 18:21:51,400.357,0x0054,0,65535,-22.3,4350,0,0,0,91,3926,4337,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1137,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4350,0,0,0,-22.4,-22.3,-22.3,4350,0,3926,1520,4337,1698,3926,1520,411,178,4337,1698,-22.1,-22.3,1000,0,0,14,0,52,2144,0,0,0,768,4889,0,0,0,10.0,417,2144,4538,1777,914,SUCCESS 41,2023-05-04 18:22:01,410.360,0x0077,0,65535,-22.3,4350,0,0,0,91,3926,4337,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1137,0x00C0,10,97,0x8300,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4350,0,0,0,-22.4,-22.4,-22.4,4350,4,3926,1520,4337,1698,3926,1520,411,178,4337,1698,-22.1,-22.3,1000,0,0,14,0,62,2144,0,0,0,768,4889,0,0,0,10.0,417,2144,4538,1777,880,SUCCESS 42,2023-05-04 18:22:11,420.374,0x0054,0,65535,-22.3,4350,0,0,0,91,3926,4337,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1137,0x00C0,10,97,0x8300,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4350,0,0,0,-22.5,-22.3,-22.3,4350,0,3926,1520,4337,1698,3926,1520,411,178,4337,1698,-22.1,-22.3,1000,0,0,14,0,72,2144,0,0,0,768,4889,0,0,0,10.0,417,2144,4538,1777,881,SUCCESS 43,2023-05-04 18:22:21,430.381,0x0054,0,65535,-22.4,4350,0,0,0,91,3926,4337,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1137,0x00C0,10,97,0x8300,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4350,0,0,0,-22.4,-22.4,-22.4,4350,-7,3926,1520,4337,1698,3926,1520,411,178,4337,1698,-22.1,-22.4,1000,0,0,14,0,82,2144,0,0,0,768,4889,0,0,0,10.0,417,2144,4538,1777,872,SUCCESS 44,2023-05-04 18:22:31,440.387,0x0054,0,65535,-22.4,4350,0,0,0,91,3926,4337,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1137,0x00C0,10,97,0x8300,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4351,0,0,0,-22.5,-22.4,-22.4,4351,0,3926,1520,4337,1698,3926,1520,411,178,4337,1698,-22.1,-22.4,1000,0,0,14,0,92,2144,0,0,0,768,4889,0,0,0,10.0,417,2144,4538,1777,930,SUCCESS 45,2023-05-04 18:22:41,450.397,0x0054,0,65535,-22.4,4350,0,0,0,91,3926,4337,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1137,0x00C0,10,97,0x8200,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4350,0,0,0,-22.5,-22.4,-22.4,4350,-11,3926,1520,4337,1698,3926,1520,411,178,4337,1698,-22.1,-22.4,1000,0,0,14,0,102,2144,0,0,0,768,4889,0,0,0,10.0,417,2144,4538,1777,951,SUCCESS 46,2023-05-04 18:22:51,460.411,0x0054,0,65535,-22.4,4351,0,0,0,91,3926,4337,65535,65535,-500,471,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1137,0x00C0,10,97,0x8100,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4351,0,0,0,-22.5,-22.5,-22.5,4351,-4,3926,1520,4337,1698,3926,1520,411,178,4337,1698,-22.1,-22.4,1000,0,0,14,0,112,2144,0,0,0,768,4889,0,0,0,10.0,417,2144,4538,1777,861,SUCCESS 47,2023-05-04 18:23:01,470.420,0x0000,0,0,19.8,0,0,0,0,0,0,4670,0,0,-996,0,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,4450,4450,0,0x00C0,10,0,0x0300,0x0040,0x00,0x0000,0x40,0x0014,0x0008,3865,-993,-384,-385,-22.5,-22.8,-22.4,3863,-993,4568,1799,4339,1698,4568,1799,-229,-101,4339,1698,-22.4,-22.4,1000,0,0,14,0,0,0,0,0,0,768,4889,0,0,0,10.0,417,0,4538,1777,928,SUCCESS 48,2023-05-04 18:23:11,480.430,0x0054,0,65535,-22.4,3847,-993,-993,-383,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1231,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3846,-993,-382,-382,-22.5,-22.4,-22.4,3844,-993,4565,1797,4339,1698,4565,1797,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,9,0,3,1,0,768,4889,0,3,0,10.0,417,0,4538,1777,888,SUCCESS 49,2023-05-04 18:23:21,490.436,0x0054,0,65535,-22.3,3834,-996,-993,-382,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1238,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3833,-993,-381,-379,-22.4,-22.3,-22.3,3832,-993,4562,1796,4339,1698,4562,1796,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,19,0,6,2,0,768,4889,0,6,0,10.0,417,0,4538,1777,882,SUCCESS 50,2023-05-04 18:23:31,500.439,0x0054,0,65535,-22.1,3824,-993,-993,-381,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1253,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3823,-996,-381,-380,-22.4,-22.1,-22.1,3823,-993,4560,1795,4339,1698,4560,1795,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,29,0,8,3,0,768,4889,0,8,0,10.0,417,0,4538,1777,893,SUCCESS 51,2023-05-04 18:23:41,510.448,0x0054,0,65535,-22.1,3816,-993,-993,-380,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1253,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3815,-993,-379,-379,-22.3,-22.1,-22.1,3815,-993,4557,1794,4339,1698,4557,1794,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,39,0,11,4,0,768,4889,0,11,0,10.0,417,0,4538,1777,905,SUCCESS 52,2023-05-04 18:23:51,520.455,0x0054,0,65535,-22.1,3809,-993,-993,-379,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1252,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3809,-996,-379,-378,-22.3,-22.1,-22.1,3808,-993,4554,1793,4339,1698,4554,1793,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,49,0,14,5,0,768,4889,0,14,0,10.0,417,0,4538,1777,878,SUCCESS 53,2023-05-04 18:24:01,530.457,0x0054,0,65535,-22.1,3803,-993,-993,-379,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1252,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3802,-993,-378,-379,-22.2,-22.1,-22.1,3802,-996,4551,1792,4339,1698,4551,1792,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,59,0,17,6,0,768,4889,0,17,0,10.0,417,0,4538,1777,876,SUCCESS 54,2023-05-04 18:24:11,540.468,0x0054,0,65535,-22.0,3797,-993,-993,-378,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1257,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3797,-989,-376,-376,-22.2,-22.0,-22.0,3796,-993,4549,1791,4339,1698,4549,1791,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,69,0,19,7,0,768,4889,0,19,0,10.0,417,0,4538,1777,911,SUCCESS 55,2023-05-04 18:24:21,550.472,0x0054,0,65535,-22.0,3793,-993,-993,-377,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1257,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3792,-989,-375,-375,-22.2,-22.0,-22.0,3792,-993,4546,1790,4339,1698,4546,1790,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,79,0,22,8,0,768,4889,0,22,0,10.0,417,0,4538,1777,925,SUCCESS 56,2023-05-04 18:24:31,560.477,0x0054,0,65535,-22.0,3788,-989,-992,-377,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1256,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3788,-993,-376,-376,-22.2,-22.0,-22.0,3787,-993,4543,1789,4339,1698,4543,1789,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,89,0,25,9,0,768,4889,0,25,0,10.0,417,0,4538,1777,888,SUCCESS 57,2023-05-04 18:24:41,570.478,0x0054,0,65535,-21.9,3784,-993,-993,-376,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1264,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3783,-989,-374,-374,-22.2,-21.9,-21.9,3783,-993,4540,1788,4339,1698,4540,1788,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,99,0,28,10,0,768,4889,0,28,0,10.0,417,0,4538,1777,887,SUCCESS 58,2023-05-04 18:24:51,580.482,0x0054,0,65535,-21.9,3780,-993,-993,-376,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1263,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3780,-993,-375,-375,-22.1,-21.9,-21.9,3779,-993,4538,1787,4339,1698,4538,1787,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,109,0,30,11,0,768,4889,0,30,0,10.0,417,0,4538,1777,898,SUCCESS 59,2023-05-04 18:25:01,590.490,0x0054,0,65535,-21.9,3777,-989,-993,-375,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1263,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3776,-993,-375,-375,-22.1,-21.9,-21.9,3776,-993,4535,1786,4339,1698,4535,1786,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,119,0,33,12,0,768,4889,0,33,0,10.0,417,0,4538,1777,875,SUCCESS 60,2023-05-04 18:25:11,600.504,0x0054,0,65535,-21.8,3773,-993,-993,-375,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1270,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3773,-993,-375,-375,-22.1,-21.9,-21.8,3773,-993,4532,1785,4339,1698,4532,1785,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,129,0,36,13,0,768,4889,0,36,0,10.0,417,0,4538,1777,891,SUCCESS 61,2023-05-04 18:25:21,610.508,0x0054,0,65535,-21.8,3770,-993,-993,-375,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1270,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3770,-993,-374,-374,-22.0,-21.9,-21.8,3769,-993,4529,1784,4339,1698,4529,1784,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,139,0,39,14,0,768,4889,0,39,0,10.0,417,0,4538,1777,890,SUCCESS 62,2023-05-04 18:25:31,620.514,0x0054,0,65535,-21.8,3767,-989,-993,-374,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1269,0x00C0,10,97,0x0200,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3767,-993,-374,-374,-22.1,-21.9,-21.8,3767,-993,4527,1783,4339,1698,4527,1783,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,149,0,41,15,0,768,4889,0,41,0,10.0,417,0,4538,1777,868,SUCCESS 63,2023-05-04 18:25:41,630.528,0x0077,0,65535,-21.7,3764,-989,-993,-374,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1276,0x00C0,10,97,0x0200,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3764,-996,-375,-120,-22.0,-22.1,-21.7,4051,-319,4524,1782,4339,1698,4524,1782,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,159,0,44,16,0,768,4889,0,44,0,10.0,417,0,4538,1777,899,SUCCESS 64,2023-05-04 18:25:51,640.537,0x0077,0,65535,-21.8,4225,0,-511,-192,100,4339,4339,509,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1269,0x00C0,10,97,0x0100,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4230,0,0,0,-22.0,-21.9,-21.8,4235,0,4524,1782,4339,1698,4524,1782,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,169,0,44,16,0,768,4889,0,44,0,10.0,417,0,4538,1777,1000,SUCCESS 65,2023-05-04 18:26:01,650.545,0x0054,0,65535,-21.8,4254,0,-257,-97,100,4339,4339,1013,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1269,0x00C0,10,97,0x0100,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4256,0,0,0,-22.2,-21.8,-21.8,4258,0,4524,1782,4339,1698,4524,1782,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,179,0,44,16,0,768,4889,0,44,0,10.0,417,0,4538,1777,883,SUCCESS 66,2023-05-04 18:26:12,660.557,0x0054,0,65535,-21.9,4266,0,-129,-49,100,4339,4339,2018,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1261,0x00C0,10,97,0x0100,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4267,0,0,0,-22.2,-21.9,-21.9,4268,0,4524,1782,4339,1698,4524,1782,-229,-100,4339,1698,-22.8,-22.8,1000,0,1,14,1,189,0,44,16,0,768,4889,0,44,0,10.0,417,0,4538,1777,902,SUCCESS 67,2023-05-04 18:26:22,670.571,0x0054,0,65535,-21.9,4272,0,0,0,83,3579,4324,65535,65535,-500,429,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,934,4450,1101,0x00C0,10,97,0x8300,0x0440,0x01,0x0018,0x40,0x0014,0x0008,4275,0,0,0,-22.2,-21.9,-21.9,4275,-4,3579,1375,4324,1694,3579,1375,745,319,4324,1694,-21.9,-21.9,1000,0,0,14,0,6,3264,0,0,0,768,4889,0,0,0,10.0,417,3264,4538,1777,934,SUCCESS 68,2023-05-04 18:26:32,680.581,0x0054,0,65535,-21.9,4278,0,0,0,83,3579,4324,65535,65535,-500,429,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1101,0x00C0,10,97,0x8300,0x0440,0x01,0x0018,0x40,0x0014,0x0008,4281,0,0,0,-22.2,-22.0,-22.0,4281,0,3579,1375,4324,1694,3579,1375,745,319,4324,1694,-21.9,-21.9,1000,0,0,14,0,16,3264,0,0,0,768,4889,0,0,0,10.0,417,3264,4538,1777,878,SUCCESS 69,2023-05-04 18:26:42,690.588,0x0054,0,65535,-22.0,4283,0,0,0,83,3579,4324,65535,65535,-500,429,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1101,0x00C0,10,97,0x8200,0x0440,0x01,0x0018,0x40,0x0014,0x0008,4285,0,0,0,-22.3,-22.0,-22.0,4285,0,3579,1375,4324,1694,3579,1375,745,319,4324,1694,-21.9,-22.0,1000,0,0,14,0,26,3264,0,0,0,768,4889,0,0,0,10.0,417,3264,4538,1777,872,SUCCESS 70,2023-05-04 18:26:52,700.603,0x0054,0,65535,-22.1,4287,0,0,0,83,3579,4324,65535,65535,-500,429,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1101,0x00C0,10,97,0x8200,0x0440,0x01,0x0018,0x40,0x0014,0x0008,4289,0,0,0,-22.3,-22.1,-22.1,4289,-7,3579,1375,4324,1694,3579,1375,745,319,4324,1694,-21.9,-22.1,1000,0,0,14,0,36,3264,0,0,0,768,4889,0,0,0,10.0,417,3264,4538,1777,935,SUCCESS 71,2023-05-04 18:27:02,710.618,0x0054,0,65535,-22.1,4291,0,0,0,83,3579,4324,65535,65535,-500,429,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1101,0x00C0,10,97,0x8100,0x0440,0x01,0x0018,0x40,0x0014,0x0008,4292,0,0,0,-22.3,-22.0,-22.0,4292,4,3579,1375,4324,1694,3579,1375,745,319,4324,1694,-21.9,-22.1,1000,0,0,14,0,46,3264,0,0,0,768,4889,0,0,0,10.0,417,3264,4538,1777,888,SUCCESS 72,2023-05-04 18:27:12,720.628,0x0000,0,0,-22.1,4294,0,0,0,0,0,4670,0,0,-500,0,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,4450,4450,0,0x00C0,10,97,0x0300,0x0040,0x00,0x0000,0x40,0x0014,0x0008,4294,0,0,0,-22.3,-22.5,-22.1,4296,0,3689,1421,4329,1696,3689,1421,640,275,4329,1696,-22.1,-22.1,1000,0,0,14,0,0,2912,0,0,0,768,4889,0,0,0,10.0,417,2912,4538,1777,893,SUCCESS 73,2023-05-04 18:27:22,730.635,0x0077,0,65535,-22.1,4296,0,0,0,86,3689,4329,65535,65535,-500,443,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1099,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4296,0,0,0,-22.4,-22.1,-22.1,4296,0,3689,1421,4329,1696,3689,1421,640,275,4329,1696,-22.1,-22.1,1000,0,0,14,0,10,2912,0,0,0,768,4889,0,0,0,10.0,417,2912,4538,1777,856,SUCCESS 74,2023-05-04 18:27:32,740.649,0x0054,0,65535,-22.1,4298,0,0,0,86,3689,4329,65535,65535,-500,443,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1099,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4298,0,0,0,-22.4,-22.1,-22.1,4298,0,-32000,64,0,0,3689,1421,640,275,4329,1696,-22.1,-22.1,1000,0,0,14,0,20,2912,0,0,0,768,4889,0,0,0,10.0,417,2912,4538,1777,966,SUCCESS 75,2023-05-04 18:27:42,750.660,0x0054,0,65535,-22.2,4300,0,0,0,86,3689,4329,65535,65535,-500,443,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1099,0x00C0,10,97,0x8200,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4300,0,0,0,-22.5,-22.2,-22.2,4300,0,3689,1421,4329,1696,3689,1421,640,275,4329,1696,-22.1,-22.2,1000,0,0,14,0,30,2912,0,0,0,768,4889,0,0,0,10.0,417,2912,4538,1777,878,SUCCESS 76,2023-05-04 18:27:52,760.662,0x0054,0,65535,-22.3,4302,0,0,0,86,3689,4329,65535,65535,-500,443,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1099,0x00C0,10,97,0x8100,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4302,0,0,0,-22.4,-22.3,-22.3,4302,0,3689,1421,4329,1696,3689,1421,640,275,4329,1696,-22.1,-22.3,1000,0,0,14,0,40,2912,0,0,0,768,4889,0,0,0,10.0,417,2912,4538,1777,892,SUCCESS 77,2023-05-04 18:28:02,770.673,0x0054,0,65535,-22.3,4304,0,0,0,86,3689,4329,65535,65535,-500,443,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1099,0x00C0,10,97,0x8100,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4304,0,0,0,-22.4,-22.3,-22.3,4304,0,3689,1421,4329,1696,3689,1421,640,275,4329,1696,-22.1,-22.3,1000,0,0,14,0,50,2912,0,0,0,768,4889,0,0,0,10.0,417,2912,4538,1777,863,SUCCESS 78,2023-05-04 18:28:12,781.060,0x0054,0,65535,-22.3,4305,0,0,0,87,3731,4333,65535,65535,-500,448,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,934,4450,1097,0x00C0,10,97,0x8300,0x0040,0x02,0x0004,0x40,0x0014,0x0008,4305,0,0,0,-22.5,-22.3,-22.3,4305,-4,3731,1437,4333,1696,3731,1437,602,259,4333,1696,-22.3,-22.3,1000,0,0,14,0,3,2784,0,0,0,768,4889,0,0,0,10.0,417,2784,4538,1777,883,SUCCESS 79,2023-05-04 18:28:22,790.685,0x0054,0,65535,-22.4,4306,0,0,0,87,3731,4333,65535,65535,-500,448,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1097,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4306,0,0,0,-22.5,-22.4,-22.4,4306,-4,3731,1437,4333,1696,3731,1437,602,259,4333,1696,-22.3,-22.4,1000,0,0,14,0,13,2784,0,0,0,768,4889,0,0,0,10.0,417,2784,4538,1777,866,SUCCESS 80,2023-05-04 18:28:32,801.064,0x0054,0,65535,-22.4,4307,0,0,0,87,3731,4333,65535,65535,-500,448,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1097,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4307,0,0,0,-22.5,-22.4,-22.4,4307,-7,3731,1437,4333,1696,3731,1437,602,259,4333,1696,-22.3,-22.4,1000,0,0,14,0,23,2784,0,0,0,768,4889,0,0,0,10.0,417,2784,4538,1777,926,SUCCESS 81,2023-05-04 18:28:42,810.700,0x0054,0,65535,-22.4,4308,0,0,0,87,3731,4333,65535,65535,-500,448,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1097,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4308,0,0,0,-22.5,-22.4,-22.4,4308,0,3731,1437,4333,1696,3731,1437,602,259,4333,1696,-22.3,-22.4,1000,0,0,14,0,32,2784,0,0,0,768,4889,0,0,0,10.0,417,2784,4538,1777,852,SUCCESS 82,2023-05-04 18:28:52,820.708,0x0054,0,65535,-22.4,4309,0,0,0,87,3731,4333,65535,65535,-500,448,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1097,0x00C0,10,97,0x8300,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4309,0,0,0,-22.5,-22.4,-22.4,4309,-4,3731,1437,4333,1696,3731,1437,602,259,4333,1696,-22.3,-22.4,1000,0,0,14,0,42,2784,0,0,0,768,4889,0,0,0,10.0,417,2784,4538,1777,860,SUCCESS 83,2023-05-04 18:29:02,830.724,0x0054,0,65535,-22.4,4310,0,0,0,87,3731,4333,65535,65535,-500,448,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1097,0x00C0,10,97,0x8200,0x0040,0x01,0x0018,0x40,0x0014,0x0008,4310,0,0,0,-22.5,-22.4,-22.4,4310,-4,3731,1437,4333,1696,3731,1437,602,259,4333,1696,-22.3,-22.4,1000,0,0,14,0,52,2784,0,0,0,768,4889,0,0,0,10.0,417,2784,4538,1777,860,SUCCESS 84,2023-05-04 18:29:12,840.726,0x0054,0,65535,-22.4,4311,0,0,0,87,3731,4333,65535,65535,-500,448,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1097,0x00C0,10,97,0x8100,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4311,0,0,0,-22.6,-22.4,-22.4,4311,-4,3731,1437,4333,1696,3731,1437,602,259,4333,1696,-22.3,-22.4,1000,0,0,14,0,62,2784,0,0,0,768,4889,0,0,0,10.0,417,2784,4538,1777,935,SUCCESS 85,2023-05-04 18:29:22,850.735,0x0054,0,65535,-22.5,4312,0,0,0,87,3731,4333,65535,65535,-500,448,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1097,0x00C0,10,97,0x8100,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4312,0,0,0,-22.6,-22.5,-22.5,4312,0,3731,1437,4333,1696,3731,1437,602,259,4333,1696,-22.3,-22.5,1000,0,0,14,0,72,2784,0,0,0,768,4889,0,0,0,10.0,417,2784,4538,1777,880,SUCCESS 86,2023-05-04 18:29:32,860.917,0x0054,0,65535,-22.5,4312,0,0,0,87,3731,4333,65535,65535,-500,448,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1097,0x00C0,10,97,0x8100,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4312,0,0,0,-22.6,-22.5,-22.5,4312,0,3731,1437,4333,1696,3731,1437,602,259,4333,1696,-22.3,-22.5,1000,0,0,14,0,83,2784,0,0,0,768,4889,0,0,0,10.0,417,2784,4538,1777,870,SUCCESS 87,2023-05-04 18:29:42,870.747,0x0054,0,65535,-22.5,4313,0,0,0,87,3731,4333,65535,65535,-500,448,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1097,0x00C0,10,97,0x8100,0x0440,0x01,0x0018,0x40,0x0034,0x0008,4313,0,0,0,-22.6,-22.5,-22.5,4313,4,3731,1437,4333,1696,3731,1437,602,259,4333,1696,-22.3,-22.5,1000,0,0,14,0,92,2784,0,0,0,768,4889,0,0,0,10.0,417,2784,4538,1777,852,SUCCESS 88,2023-05-04 18:29:52,880.949,0x0054,0,65535,-22.5,3975,0,0,0,87,3731,4333,65535,65535,-500,448,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1097,0x00C0,10,97,0x8100,0x0440,0x01,0x0014,0x40,0x0034,0x0008,3975,0,0,0,-22.5,-22.5,-22.5,3975,-993,3731,1437,4333,1696,3731,1437,602,259,4333,1696,-22.3,-22.5,1000,0,0,14,0,103,2784,0,0,0,768,4889,0,0,0,10.0,417,2784,4538,1777,868,SUCCESS 89,2023-05-04 18:30:02,890.763,0x0054,0,65535,-22.5,3812,-993,-995,-381,87,3728,4333,225,65535,-996,225,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1084,0x00C0,10,97,0x0100,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3812,-993,-379,-379,-22.5,-22.5,-22.5,3810,-993,3728,1434,4333,1694,3723,1434,602,259,4328,1694,-22.5,-22.8,1000,0,2,14,2,6,2784,3,1,0,768,4889,0,3,0,10.0,417,2784,4538,1777,882,SUCCESS 90,2023-05-04 18:30:12,900.998,0x0054,0,65535,-22.4,3796,-993,-993,-377,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1232,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3794,-993,-377,-377,-22.5,-22.4,-22.4,3793,-993,4567,1799,4339,1698,4567,1799,-229,-101,4339,1698,-22.0,-22.7,1000,0,1,14,1,4,0,1,0,0,768,4889,0,1,0,10.0,417,0,4538,1777,914,SUCCESS 91,2023-05-04 18:30:22,910.777,0x0054,0,65535,-22.3,3785,-996,-993,-377,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1238,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3785,-996,-377,-377,-22.4,-22.3,-22.3,3784,-993,4564,1798,4339,1698,4564,1798,-229,-101,4339,1698,-22.0,-22.7,1000,0,1,14,1,13,0,4,1,0,768,4889,0,4,0,10.0,417,0,4538,1777,869,SUCCESS 92,2023-05-04 18:30:32,920.788,0x0054,0,65535,-22.3,3777,-989,-992,-376,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1238,0x00C0,10,97,0x0200,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3777,-993,-375,-374,-22.4,-22.3,-22.3,3776,-993,4561,1797,4339,1698,4561,1797,-229,-101,4339,1698,-22.0,-22.7,1000,0,1,14,1,23,0,7,2,0,768,4889,0,7,0,10.0,417,0,4538,1777,919,SUCCESS 93,2023-05-04 18:30:42,930.792,0x0054,0,65535,-22.2,3770,-993,-992,-375,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1245,0x00C0,10,97,0x0200,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3770,-989,-373,-374,-22.3,-22.2,-22.2,3770,-993,4559,1796,4339,1698,4559,1796,-229,-101,4339,1698,-22.0,-22.7,1000,0,1,14,1,33,0,9,3,0,768,4889,0,9,0,10.0,417,0,4538,1777,902,SUCCESS 94,2023-05-04 18:30:52,940.802,0x0054,0,65535,-22.1,3765,-993,-992,-374,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1253,0x00C0,10,97,0x0100,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3765,-996,-375,-374,-22.3,-22.1,-22.1,3764,-993,4556,1795,4339,1698,4556,1795,-229,-101,4339,1698,-22.0,-22.7,1000,0,1,14,1,43,0,12,4,0,768,4889,0,12,0,10.0,417,0,4538,1777,922,SUCCESS 95,2023-05-04 18:31:02,950.805,0x0054,0,65535,-22.1,3760,-993,-993,-374,100,4339,4339,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1252,0x00C0,10,97,0x0100,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3760,-993,-373,-373,-22.3,-22.0,-22.1,3760,-993,4553,1794,4339,1698,4553,1794,-229,-101,4339,1698,-22.0,-22.7,1000,0,1,14,1,53,0,15,5,0,768,4889,0,15,0,10.0,417,0,4538,1777,857,SUCCESS 96,2023-05-04 18:31:12,960.809,0x0054,0,65535,-22.1,3757,-993,-993,-373,100,4336,4336,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1255,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3757,-993,-373,-373,-22.3,-22.1,-22.1,3756,-993,4563,1797,4336,1696,4563,1797,-229,-101,4336,1696,-22.5,-22.5,1000,0,1,14,1,6,0,2,0,0,768,4889,0,2,0,10.0,417,0,4538,1777,852,SUCCESS 97,2023-05-04 18:31:22,970.823,0x0054,0,65535,-22.1,3753,-993,-993,-373,100,4336,4336,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1254,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3753,-993,-373,-373,-22.3,-22.1,-22.1,3752,-993,4561,1796,4336,1696,4561,1796,-229,-101,4336,1696,-22.5,-22.5,1000,0,1,14,1,16,0,5,1,0,768,4889,0,5,0,10.0,417,0,4538,1777,854,SUCCESS 98,2023-05-04 18:31:32,980.839,0x0054,0,65535,-22.0,3749,-989,-992,-372,100,4336,4336,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1261,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3749,-996,-373,-371,-22.3,-22.0,-22.0,3749,-993,4558,1795,4336,1696,4558,1795,-229,-101,4336,1696,-22.5,-22.5,1000,0,1,14,1,26,0,7,2,0,768,4889,0,7,0,10.0,417,0,4538,1777,871,SUCCESS 99,2023-05-04 18:31:42,990.849,0x0054,0,65535,-22.0,3746,-993,-992,-372,100,4336,4336,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1259,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3746,-993,-372,-372,-22.2,-22.0,-22.0,3746,-993,4555,1794,4336,1696,4555,1794,-229,-101,4336,1696,-22.5,-22.5,1000,0,1,14,1,35,0,10,3,0,768,4889,0,10,0,10.0,417,0,4538,1777,859,SUCCESS 100,2023-05-04 18:31:52,1000.860,0x0054,0,65535,-21.9,3743,-993,-993,-372,100,4336,4336,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1266,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3743,-996,-373,-372,-22.2,-21.9,-21.9,3743,-989,4552,1793,4336,1696,4552,1793,-229,-101,4336,1696,-22.5,-22.5,1000,0,1,14,1,45,0,13,4,0,768,4889,0,13,0,10.0,417,0,4538,1777,880,SUCCESS 101,2023-05-04 18:32:02,1010.866,0x0054,0,65535,-21.9,3741,-993,-992,-372,100,4336,4336,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1266,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3741,-993,-371,-371,-22.2,-21.9,-21.9,3741,-993,4550,1792,4336,1696,4550,1792,-229,-101,4336,1696,-22.5,-22.5,1000,0,1,14,1,55,0,15,5,0,768,4889,0,16,0,10.0,417,0,4538,1777,890,SUCCESS 102,2023-05-04 18:32:12,1020.880,0x0054,0,65535,-21.8,3739,-993,-992,-371,100,4336,4336,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1275,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3739,-993,-371,-371,-22.1,-21.7,-21.8,3739,-993,4547,1791,4336,1696,4547,1791,-229,-101,4336,1696,-22.5,-22.5,1000,0,1,14,1,65,0,18,6,0,768,4889,0,18,0,10.0,417,0,4538,1777,875,SUCCESS 103,2023-05-04 18:32:22,1030.886,0x0054,0,65535,-21.6,3738,-996,-993,-371,100,4336,4336,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1289,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3738,-996,-372,-372,-21.9,-21.6,-21.6,3738,-993,4544,1790,4336,1696,4544,1790,-229,-101,4336,1696,-22.5,-22.5,1000,0,1,14,1,75,0,21,7,0,768,4889,0,21,0,10.0,417,0,4538,1777,884,SUCCESS 104,2023-05-04 18:32:32,1040.896,0x0054,0,65535,-21.4,3737,-993,-993,-371,100,4336,4336,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1303,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3737,-993,-371,-371,-21.8,-21.3,-21.4,3737,-993,4541,1789,4336,1696,4541,1789,-229,-101,4336,1696,-22.5,-22.5,1000,0,1,14,1,85,0,24,8,0,768,4889,0,24,0,10.0,417,0,4538,1777,891,SUCCESS 105,2023-05-04 18:32:42,1050.910,0x0054,0,65535,-21.1,3737,-993,-993,-371,100,4336,4336,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1328,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3737,-993,-371,-371,-21.5,-21.1,-21.1,3737,-993,4539,1788,4336,1696,4539,1788,-229,-101,4336,1696,-22.5,-22.5,1000,0,1,14,1,95,0,26,9,0,768,4889,0,26,0,10.0,417,0,4538,1777,876,SUCCESS 106,2023-05-04 18:32:52,1060.915,0x0054,0,65535,-20.9,3738,-993,-993,-371,100,4336,4336,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1344,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3738,-993,-371,-371,-21.2,-20.9,-20.9,3738,-993,4536,1787,4336,1696,4536,1787,-229,-101,4336,1696,-22.5,-22.5,1000,0,1,14,1,105,0,29,10,0,768,4889,0,29,0,10.0,417,0,4538,1777,856,SUCCESS 107,2023-05-04 18:33:02,1070.924,0x0054,0,65535,-20.7,3739,-993,-993,-371,100,4336,4336,262,65535,-996,261,4580,4380,2350,2550,65,60,-25,-20,1,150,175,0x00,0,0,1358,0x00C0,10,97,0x0300,0x0040,0x01,0x0012,0x40,0x0014,0x0008,3739,-993,-371,-371,-20.9,-20.6,-20.7,3739,-993,4533,1786,4336,1696,4533,1786,-229,-101,4336,1696,-22.5,-22.5,1000,0,1,14,1,115,0,32,11,0,768,4889,0,32,0,10.0,417,0,4538,1777,880,SUCCESS