1、现在很多点焊电源的全桥逆变频率是1kHz的,请问TI的工程大师们,UCC3895能在1kHz的频率下工作吗?如果不能,有没有一些比较好的方案?
2、使用外部同步信号可行吗?如果可以是不是把1kHz的信号从6脚引入就可以了?7脚上的CT还要接振荡器定时电容吗?8脚还要接振荡器定时电阻吗?
3、外部同步信号的幅值要不要限制在1.9~2.1v之间?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,根据datasheet ucc3895 min frequency is about 80Khz,但我以前用过50khz 也是没问题的,但是1khz 估计不可以,我帮你问问AE同事。
外同步也是要接 RT ,CT的。
外同步信号要大于2.1V,根据datasheet是识别高电平 2.1V,低电平 1.9V,因此需要大于2.1V,谢谢。
您好,我想请问一下,ucc3895的SYNC管脚作为输出时,datasheet上说,输出电压应该是4V左右的方波,但是我实际做实验中发现输出电压才2V,而且输出不是方波,是一个类似与电容放电的三角波,请问会是什么原因造成的?非常感谢!