这款LM3447PDF里面的Typical Primary Side Power Regulated Flyback LED Driver的隔离变压器异名输出端是要和前面共地吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这款LM3447PDF里面的Typical Primary Side Power Regulated Flyback LED Driver的隔离变压器异名输出端是要和前面共地吗?
嗯,这两个地是隔离的,作为隔离输出有几个好处:1.把输入输出地回流分开降低地上的干扰 2. 有效降低了共模噪声 3. 更加的安全
如XP所说,一般接一个Y电容即可。
我前段时间试了下用LM3447做个可调光的LED恒流源,但是我输入用的是48V,然后我根据48V的输入改了电路一些器件的参数,结果LM3447的GATE脚有PWM输出,大概是50KHZ左右平均电压5V多,但是整体的电路就是没有输出,始终没能理解,隔离变压器是自己做的,就算有误差,但是应该也有输出才对
1. 芯片PWM有输出,开关管漏极是否有对应的PWM电压?
2.变压器的输出端是否有PWM电压?
如果要做进一步分析,可以上传原理图。
谢谢