Other Parts Discussed in Thread: LM1117
由于需要5V的电压作为基准电压,使用了LM1117,电路都是按照规格书来做的,原边4个25V/10uF的陶瓷电容,输出2个25V/10uF的陶瓷电容。
由于只是做基准,负载电路很小,大约只有5mA.现在出问题了,在常温的时候,5.0V,很准确,但是到了-40度,输出电压只有4.81V,
规格书的变化率很小啊,求解决方法?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM1117
由于需要5V的电压作为基准电压,使用了LM1117,电路都是按照规格书来做的,原边4个25V/10uF的陶瓷电容,输出2个25V/10uF的陶瓷电容。
由于只是做基准,负载电路很小,大约只有5mA.现在出问题了,在常温的时候,5.0V,很准确,但是到了-40度,输出电压只有4.81V,
规格书的变化率很小啊,求解决方法?
楼主看一下你的电容,在温度到 -40度时容值会变到多少。
电容用的是TDK的X7R系列,-55度到125度。低温容量变化约10%。尝试过增加一倍电容,输出电压在低温下还是4.8V左右,没什么变化
Hi LiangPing,
根据您的描述,测试像是使用了万用表直接测量输出电压。建议使用过示波器去观测输出电压的变化。
这样可以分辨输出电压是否是由于温度降低导致输出电压纹波变大,结果平均电压降低,确认是否是稳定性问题。
谢谢。
如果把LM1117换成LP2980怎么样?这个对容性要求要求蛮低的,陶瓷电容也可以用,精度也不错。