请推荐一款DC-DC升压IC,输入10-60V,恒压最大输出60V,恒流2-5A可调,有过流保护和短路保护功能。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1 输入一直小于42V,输出一直大于等于42V对吧?
2 请问恒流对精度是否有要求?恒流可调是需要使用单片机调节?
3 输入是锂电池组?输出是锂电池组?如果都是锂电池,是否考虑均衡充电?均衡对于锂电池组很重要。
谢谢.
可以使用TPS40211里面的LED驱动的方式来做。
不过有几点要注意
1. 输入输出不能共地。
2.电池组的安全需要而外的器件做保护。
3.单纯的boost不具备短路保护的能力。
也可以采用LM5022一类的设计为sepic电路来做,可以共地,有短路保护的功能,提高电流精度需要额外的运放来实现。
Hi
用TPS40211时,因为输出功率比较大,需要额外增加驱动芯片的。