如标题,请帮忙解释下和推荐下相应的温度,项目需求,在温漂和精度上要求比较高;输入电压是15V,输出是8V,电流最大不会超过100mA,要求温漂性能好,且精度高,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
你需要的精度是多少? 一般LDO输出精度在2%左右,即便考虑到温漂也不会特别有影响。
关于温度,你需要考虑芯片的热阻,和环境温度。 芯片的结温是环境温度加上热阻*功耗,一般不建议超过100℃,当然温度相对较低一些更好。
Hi
如果是这样的话,只能在LDO list中找合适规格的芯片(输入电压,电流满足, 热阻尽量小的LDO)
然后在在LDO datasheet里面找温漂尽量小的LDO. (比较麻烦,只能逐个查找datasheet来选择)