charger的0X05寄存器在适配插入的时候会自动配置一个值,这个值是根据什么配置的?有什么依据吗?这个寄存器能不能关闭自动配置改成手动配置?
在接电脑的HUB充电时遇到过charger把VBUS拉低至4.1V的情况,这个电压远低于我们预想的值。请问是否能在适配器插入后重新配置这个寄存器的值,保证输入电压在我们预设的范围,比如设置0X05为4.6V,这样做是否符合规范?
目前我们采用在适配器插入后重新配置0x05,但是发现还是有出现REG0X05寄存器配置的4.6V,但是VBUS却低于4.1V的情况,这个是否符合预期?是否会有其他的配置和这个冲突?或者说在什么情况下这个寄存器的配置会失效?