大家好!我现在板子上的+-25V用DC POWER supplyDF1731SL3A提供,再用7815和7915降压+-25V提供+-15V。但是板子测试的电源噪声在Vp-p=10MV,而且有很大的毛刺。我现在需要噪声极低的电源方案来做精密测量,这样电源显然太差。但是板子用的OPA551又需要+-25V的供电电压,另一组运放则+-15V供电。既满足高电压又极低噪声的电压源而且输出双极性供电。。。。
下图为用LM7815和LM7915的电源方案的地噪声
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS7A33 PSRR:64dB, output noise:16uVrms input voltage:-3~-36V
TPS7A49 PSRR:53dB, output noise:12.7uVrms input voltage:+3~+36V
你好,首先注意测量方法的正确性,其次,可以考虑使用TPS7A4901 和TPS7A3001, 高PSRR ,低噪声,谢谢。
如果我要对这样的电压源芯片做噪声仿真,我应该选择瞬时仿真吗?输入用什么样的噪声源仿真?还是有别的方法,主要我想仿真看到电源芯片电源在利用DC POWER SUPPLY电源供电后的噪声Vp-p
我在设计TPS7A4901和TPS7A3001时,知道DC/DC电源容易有噪声,得前后加LC滤波和磁珠滤波,我的使用环境要求板子的电源噪声一定要很低。但是我又不清楚如何针对TPS7A4901和TPS7A3001设计LC以及如何选择磁珠。请问TI是否有相应的参考文献或者建议