如题,CVDD0输出电压是正确的,输出电流很大,测量静态电阻是3.6欧。但是一上电,输出电流就直接会到达10A以上,请问这是什么原因?
附件中是9244的工程。附图是原理图。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
今天用电源直接接到了CVDD0的两端,测的电流是1.5A左右。
我们是12V电源输入,9244未工作时是0.6A,9244上电后是0.9A左右。然后用将CVDD0单独用1V电源接出,12V电源输入的电流为0.8A左右,1V电源的电流是1.5A左右。
刚开始未考虑从功率上进行判别。现在看来,CVDD0的实际电流应该是1.5A左右。如果是10A,那么12V电源的电流就应该有1.5A以上,所以现在看来,后端的电路应该是没有问题的。
但是现在的问题是,我使用的工程和上一板的一样,而且这一部分的电路也没有修改。但是显示的电流要比实际的电流大10倍左右。这是因为什么造成的?需要调节IOUT_CAL_GAIN这个电阻么?
我们的7242的IMON和9244的CS之间用了100欧的电阻,这个会有影响么?我在网上看说的这个推荐直接相连的。还是说需要调节IMON与模拟地之间的那个电阻?