大家好,我现在的板子需要两对电源轨,+-30V和+-15V。利用DC POWER SUPPLY供电。由于板子用于精密测量,所以要求电源的噪声小于5MV。看过很多贴,所利用DC/DC电源降压,再加二级LC滤波,可得到较低噪声电源,但LC容易振荡,而且设置复杂。所以我相利用LDO来做电压降噪。如下图1。但是我查阅相关资料,好像LDO(我选的是TPS7A4901和TPSa3001将+-36V降压到+-15V)如果调节的压差很大,会产生发热严重的问题。所以我想先利用DC/DC开关电压调解器,将+-36V降压到+-15V,在利用LDO处理输出噪声。如下图2
请问大家看看我上面的想法有什么问题没有?LDO处理电源噪声一定比LC滤波好么?如果我的图2的设计没有问题,能否给出最合适的DC/DC芯片型号(要求低噪声,负载电流1A以上)?图2后面的LDO依然用TPS7A4901和TPSa3001来对+-15V电压降噪是否最合适?
(图1)
(图2)