This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于电量监控芯片BQ34Z11OPW的使用疑问

你好,请问如果我要监控由两个12V铅酸电池串联成的24V蓄电池,参考的设计电路是按照 使用手册上的  Figure 7 2-cell lead-acid  设计,还是参考Figure 8 multi-cell lead-acid ;   还有一个问题是I2C通信口如果没有串接100R电阻和稳压二极管会烧掉后面接的ARM芯片吗?  我后面电路的I2C用的是3.3V电压,与BQ34Z11OPW的I2C接口直接相连,会经常烧掉后面的ARM芯片,请问怎么处理?

  • 你好请参考Figure 8 multi-cell lead-acid  的电路图,参考Figure 2 2-cell lead-acid  不适合于贵司该项目。谢谢!

  • 稳压管和两边的100欧姆电阻构成一个ESD保护电路,防止在插拔或其他金属接触时放电时打坏器件,建议是加入该保护电路的,否则系统的通讯会很脆弱。谢谢!

  • 1)请问 Figure 8中的BAT-和PACK-分别是指什么,对于我用两节12V铅酸电池串联来说,都是指第二节电池的负端吗?

    2)Figure 8 中的SW1,Q4,Q5是必须要的器件吗,请问SW1的作用是什么呢,如果这几个器件没加,会有什么后果?

  • BAT-指的是电芯组的地,PACK-指的是整个电池包的地,通常PACK-回连接到系统板的地。

    分压电路会带来比较大的功耗,Q4,Q5的作用是只有在34Z110需要读取电压时才使能分压电路,达到一个低功耗的目的。SW1是用来使能LED等显示的。(VEN是一个复用功能的管脚)

  • 1)你好,我的蓄电池是由上图所示两个12V电池串联组成的,BAT+是1脚,BAT-和PACK-都是指4脚吗,还是BAT-指2脚,请回复,谢谢!

    2) VEN的使能是芯片自己控制的,与SW1开关无关,对吗?还是当SW1闭合后,VEN会一直被拉高,手册上说REG25脚是2.5V的输出电压;

    3)SW1是一个带LED指示灯的开关吗,是用来指示芯片是否在读取外部电压用,还是有其它的用途,

    问题比较多,我们的项目也很着急,请工程师尽快回复,谢谢!

  • 1)BAT-是4脚, PACK-和BAT之间只连接了采样电阻, 2脚对于34z芯片没有使用到,

    2)VEN的分压控制是芯片自己使能的。SW1闭合后VEN是会一直被拉高

    3)SW1闭合后,REG25上电压加到VEN上能够提供一个信号给芯片,是芯片进行LED现实。(LED现实是显示电池包的电量值)