这个芯片的作用是什么呢???求大神给讲解下这个电路~~~~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
当电池电压比设定的输出电压3V低的时候,boost电路开始工作,将低于3V的电池电压升压到3V,按照电路图设计者的意图,是可以进一步的扩大电池单次充饱以后的使用时间。
需要说明一点:大多数的单节锂聚合物电池放电到3V以后 是要进行过放保护的,如果锂电池进一步放电到低于3V以上,对电池的寿命有损害。所以通过锂电芯的保护模块会侦测电池电压低于3V时切断放电回路以免影响电池整体寿命。
基于此,建议楼主: 查该电芯的datasheet,找到其放电曲线中过放的门限电压,一般是标写的2.7V,电池保护芯片为了确保电池的电压不会低于2.7V,所以选择高一点的3V作为放电截止门限。但这部分电压(3.0V至2.7V)之间对应的电量如果强行要升压使用,考虑到升压过程中的功率损失,带来的效益并不明显,。如果datasheet给出该电池的放电截止门限可以放到很低,那么采用TPS61200才有意义,但从给出的标称电压来看是一般的锂聚合物电池而非锂铁电池。谢谢!
您好,这个电路的作用是保证后面的系统电压不会低于3V,即使电池电压低于3V 。
如果你是锂电池供电,而且后级需要较大的电流,建议使用TPS61280,专用于电池前端,用于保证输出电压不会低于某个值。
TPS61280相比TPS61220的优势是,280具有bypass的功能,在不升压的时候输入输出压降很小。
相比一般的锂聚合物电池,我个人认为在磷酸铁锂电池的情况下需要这样的boost电路,如果是常规的标称3.6、3.7V的锂电池,加入这个升压转换器的意义不大。除非楼主的项目非常强调单次充电后的使用时间,即使牺牲电池的使用寿命也愿意。以上谢谢!