This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TI芯片SOH的定义标准



SOH在计量芯片中用0~100的值表示电池健康状态,请问这个参数对客户来说,有没有比较直观的表达?是不是SOH到0%的时候表示电池寿命已尽,还是说FCC用到80%时表示SOH是0%,请大神解释一下SOH在TI计量芯片中的具体定义。谢谢~

  • SOH是标准状况下的FCC数值除以设计容量,标准状况就是指25度,负载为SOH电流(Dataflash参数配置)。一般而言当SOH下降到70%-80%的时候,电池就会进入一个急剧老化的状态,有的厂商会在此时对电池做报废处理提示客户更换电池。

  • 恩,明白了,非常谢谢。如果客户不知道电池多大容量,也就是无法确定DESIGN CAPACITY,那在未完全充放电情况下,IC能自动学习电池容量吗?还是充放电一次IC就知道了?

  • 理论上阻抗跟踪电量计只要求有准确的CHEM-ID,通过充放电静置过程就可以学习到电池容量,不需要填入具体设计容量,但是部分参数会以设计容量作为一个更新门限值或者比例数值(尤其BQ274XX系列的),所以虽然不要求填入十分精确的设计容量,但是这个数值不要偏离太多。