我是通过MCU输出1kHz的PWM信号经过RC滤波得来的电平信号,给TPS92641的IADJ端提供模拟信号控制输出电流的。在这个测试的过程中我发现,即使我把PWM的duty调到0%,LED还是会有微弱的亮光,无法彻底关断。具体原理图如下
此外还有一个问题,就是发热很严重,能从哪方面改善效率低下的问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
驱动电阻尽量小, 可以不要。(15ohm太大)。
芯片发热,可以选择Qg尽量小的MOS, 以及适当的降低频率,这些都影响效率。另外Powerpad的散热设计要特别注意。
调光0V输入,有可能有非常微弱的电流是正常的。