Dear all
给TPS65020 第7脚施加-0.07V电压后,再次开电,有部分TPS65020 不工作,请问是什么原因。之前的几批TPS65020按照同样的测试方法都是没有问题的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all
给TPS65020 第7脚施加-0.07V电压后,再次开电,有部分TPS65020 不工作,请问是什么原因。之前的几批TPS65020按照同样的测试方法都是没有问题的。
1.请问你是为何要在7脚加0.7V的电压?
2.这个0.7V电压是瞬间的还是直流的?
3.不工作的芯片现象是什么?
谢谢
请问 -0.07V是怎么加到芯片的,从那两个脚加入的?
-0.07V又是如何产生的。
The -0.07V is a leak current from additional port logic working with -12V,
您好,
在芯片的任意两个引脚接入-0.07V,都是不会损坏芯片的。
如果系统中有高压,请检查在瞬态特性下,芯片引脚电压有没有超过最大耐压的情况。
请检查是否由于ESD特性导致的器件损坏。
谢谢
您好,
1 芯片的Absolute Maximum Ratings 的-0.3V是芯片内部的寄生体二极管决定的,高电压由芯片内部管子击穿或者工作不正常决定的。
2 可以参考附件来看Absolute Maximum Ratings。
3 可以申请我们的样片实际测试一下。
谢谢
你好,芯片使用最好用在推荐值,最大值可能会产生出现问题也可能不会。这里-0.07V加入的条件是否相同,可以比对一下,谢谢。