This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ29700可编程阈值问题



BQ29700可以编程阈值和定时器时间,问题如下

问题1:请问如果不进行编程操作,按照初始状态在电路中进行使用,过度充电检测(OVP) 、过度放电检测(UVP) 、充电过流检测(OCC)、放电过流检测(OCD)、负载短路检测(SCP)、对应定时器的默认值是多少?

问题2:如何进行编程操作?

  • 1. bq29700 并没有编程的功能。

    2.OVP UVP OCC, OCD的检测均为芯片内部固定值,bq297xy 为系列产品,可根据您具体要求选择不停的型号。

    参见datasheet

    http://www.ti.com/lit/ds/symlink/bq29700.pdf

  • BQ29700不能对充电过流检测(OCC)、放电过流检测(OCD)的电流值进行修改吗?有没有哪些充电过流检测(OCC)、放电过流检测(OCD)比较小的芯片?

  • 参见选型表

    6 Released Device Configurations

    PART NUMBEROVP (V)OVP DELAY (s)OVP REC DELAY (ms)UVP (V)UVP DELAY (ms)UVP REC DELAY (ms)OCC (V)OCC DELAY (ms)OCC REC DELAY (ms)OCD (V)OCD DELAY (ms)OCD REC DELAY (ms)SCD (V)SCD DELAY (µs)
    bq29700 4.275 1.25 12 2.800 144 8 0.100 8 8 0.100 20 8 0.5 250
    bq29701 4.280 1.25 12 2.300 144 8 0.100 8 8 0.125 8 8 0.5 250
    bq29702 4.350 1 12 2.800 96 8 0.155 8 8 0.160 16 8 0.3 250
    bq29703 4.425 1.25 12 2.300 20 8 0.100 8 8 0.160 8 8 0.5 250
    bq29704 4.425 1.25 12 2.500 20 8 0.100 8 8 0.125 8 8 0.5 250
    bq29705 4.425 1.25 12 2.500 20 8 0.100 8 8 0.150 8 8 0.5 250
    bq29706 3.850 1.25 12 2.500 144 8 0.150 8 8 0.200 8 8 0.6 250
    bq29707 4.280 1 12 2.800 96 8 0.090 6 8 0.090 16 8 0.3 250
  • BQ29700是通过V-检测两个mos的电压与OCC的关系来判断是否过流?V-连接的电阻是否也会影响检测?