Other Parts Discussed in Thread: LM3409, LM3409HV
我准备使用LM3409作一个开关恒流源,为充电器充电,前级整流之后的电压大概是60V左右,偶尔会在48~70之间波动,电池为32节镍氢电池,充电电流快充2A,涓流500mA,不知道LM3409产生的电流能不能符合给电池充电的要求,电流精度怎么样,我看到3409有模拟调光功能,它的电流调节幅度有没有这么大。如果这个方案不行的话有没有其他的芯片方案可以推荐,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.对于60V输入来说,应选用LM3409HV。
2. LM3409HV的模拟调光比为250:1, 完全能满足快充2A,小电流500mA的充电需求。
3. L对于22~75V输入,17V2.3A输出的典型应用,LM3409HV在全输入电压范围内,电流偏差小于5%。
以下是一个输入48Vdc~70Vdc,输出42Vdc/1.5A的设计,你可以参考一下
Hi
将电路图传上来看一下? (有标注零件型号,和测试条件)
芯片没有问题,可以再确认一下是否是电感质量问题?