Other Parts Discussed in Thread: LM3150
你好!
最近在用TI LM3150搭建从+24V到+12V和从+12V到+5V的电源模块,主要是+24V到+12V这部分电路遇到;
+24V到+12V电源模块的需求如下:
1、输入电压范围+19V~+35V,目前用+24V电源适配器做调试;
2、输出+12V/4A;
电路如附件所示,都是用wenbench产生的,但在调试中发现+24V到+12V这部分电路有如下问题:
1、+24V到+12V这路输出接了20欧电子负载,+12V到+5V这路输出接了2.5欧电子负载;开机几十秒钟内,LM3150和MOS管发烫厉害;测量了开关频率在290KHz左右,但波形不稳定,会跳动;而+12V到+5V这部分电路不会发烫,开关频率也是290KHz左右,但波形是稳定不动的。即使我把+5V输出的负载去掉,、+24V到+12V这部分的LM3150也发热厉害;
2、我试着把R26(Ron)加大到531K,发热情况会改善很多,但开关频率还是在290KHz左右,而且波形还是不稳定,会跳动;
请问:为什么修改了Ron的值,开关频率不会改变,而且波形不稳定,但+12V到+5V这部分是稳定的?是否电路上有设计错误的地方?
非常感谢大家的指导!