This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于充电芯片BQ24013A的问题咨询

Other Parts Discussed in Thread: BQ24013

目前使用BQ24013A充电管理芯片,有些问题咨询一下,希望能得到解答。

实际连接情况:

1,, 充电电压9~12V,给7.4V电池充电;

2,PIN13-cell引脚通过10K电阻上拉至充电口-----设置充电输出为两节电池充电;

3,PIN8-ISET1和PIN9-ISET2 通过7.5K电阻下拉到地-----设置充电电流最大1.3A;

4,TS管脚连接电池NTC,并通过芯片推荐的9.31K和442K电阻进行分压。

问题现象:

【1】稳压源设置9V输出,1.3A限流,接入充电口,但是不接电池,PIN19-STA2有时输出高,有时输出低,导致板上指示灯有的亮,有的不亮,现象不一致,是为什么?

【2】将电池放电到电压6.8V左右:

          (1)通过专用9V/2.5A的适配器,适配器发生过流保护,不进行充电;

            (2)   但是利用稳压源9V输出,1.3A限流充电,则可以进行充电,电流1.3A充一段时间(小于1分钟)后,在使用步骤(1)的适配器可充电;

          (3)若直接用稳压源9V输出,2.5A限流充电,发现充电电流会达到2~2.5A,在小于1分钟的时间内,恢复1.3A充电。

【3】有无可能是NTC部分的监测不准导致上述现象?如果不将电池的NTC管脚接入到芯片的TS管脚,那么芯片手册上推荐的9.31K和442K电阻应该换成多少合适?

盼复,谢谢!